ind-rmt-detergent-production

Solids Volume Measurement in Detergent Production

ind-rmt-detergent_production_general_info

General Process Information

Detergents are manufactured using a synthetic surfactant in place of the metal fatty acid salts that are used in soaps. Most of the powder detergents have soap in their mixture of ingredients, however it generally functions more as a foam depressant than as a surfactant.

Powder detergents are manufactured using various processes, such as spray drying, agglomeration, dry mixing or a combination of these.

ind-rmt-spray_drying_process

Spray Drying Process

The different stages / operations performed in a spray drying process, are: Dry (Sodium sulphate, Sodium tripolyphsophate (STP), Zeolite and others) and liquid ingredients are first combined into a slurry, or thick suspension, in a tank known as crutcher.

The slurry is heated and then pumped to the top of a tower where it is sprayed through nozzles (under high pressure) to create small droplets. The droplets fall through a current of hot air, thereby forming hollow granules as they dry. Collected from the bottom of the spray tower, the dried granules are screened to obtain a relatively standard size.

Traditional spray drying process produces relatively low-density detergent powders. Advancements in technology have enabled the soap and detergent manufacturers to reduce the air inside the granules during spray drying to obtain higher densities. The high-density detergent powders can be packed in much smaller packages than those needed previously.

ind-rmt-agglomeration

Agglomeration

Agglomeration is detergent powder manufacturing chemical technique that results in high-density powders. The process involves blending of dry raw materials with liquid ingredients. The technique involves machines such as liquid binder, rolling or shear mixing devices that cause the ingredients to collide and adhere to each other, producing larger particles.

ind-rmt-dry_mixing

Dry Mixing

Dry mixing is a detergent powder manufacturing technique, which is used to blend dry raw materials. The technique may also involve the addition of small quantities of a liquid.

ind-rmt-detergent_finished_product

Finished Product

Application: The final product is stored in silos before being packed and shipped.

Challenges: Accurately measuring the inventory of the final product is a continuous necessity for operators. The Rosemount 3D Solids Scanner accurately measures the volume of the contents inside the silos, giving operators better control over inventory management and delivery schedules, and enhances the reliability of related financial reporting.

Please enable JavaScript to use this website.