Emerson’s Smart Wireless network delivers improved furnace operations, safety for Ternium Siderar at Argentine steel plant

Rosemount® wireless transmitters measure and transmit data for determining pig iron levels in furnace hearth despite harsh conditions and saving 50% over wired alternative

AUSTIN, TX (May 27, 2010) – Emerson Process Management’s Smart Wireless network is helping deliver improved furnace operation and safety at Ternium Siderar’s steelmaking facility in San Nicolás Argentina while realizing 50 percent installed cost savings compared to a wired solution.

Emerson’s self-organizing wireless network delivers reliable electromotive force (EMF) data directly to a plant SCADA despite harsh conditions that include temperatures as high as 60° Celsius and high electromagnetic noise. The EMF measurements enable Ternium to calculate the amount of pig iron in the hearth, enabling smoother and safer furnace operations.

“We’ve improved furnace energy efficiency, process stability, and safety,” said Esteban Pagliero, Ternium Siderar electronic engineer. “Knowing the EMF enables calculation of the amount of iron and slag inside the hearth, enabling the improved operations. This allows us to avoid raising the operation level by too much which considerably increases the risk of serious accidents. “

Five Rosemount® 648 transmitters collect and send data from electrodes soldered near tapholes onto the hearth’s shell. The devices transmit continuous data to a Smart Wireless Gateway, located 50 meters away in another room, which sends the information to the facility’s SCADA.

Ternium uses Emerson’s AMS™ Suite predictive maintenance software to manage the new devices, which enables technicians to configure them, run diagnostic checks, and monitor alarms and alerts.

The Smart Wireless solution saved Ternium startup time and money. The company would have had to install a wired solution during multiple routine maintenance stoppages of its furnace, which occur every two months. Wires were also impractical because of the high temperatures in the steel runner and the network layout needed.

“Smart Wireless decreased our installation costs and time considerably,” said Pagliero. “We gained a 50 percent installed cost savings with the wireless solution.” 

Wireless also made it much easier and quicker for Ternium to relocate electrodes on the hearth to detect the best possible EMF signal.

“Wireless technology provided us with the ability to easily move the transmitters whenever we needed to move the electrodes. It would have taken months to do so with a wired network,” Pagliero said. “The entire installation would have taken six months in all. Installation and start-up with wireless, including finding the optimal location for the process measurement, was completed in seven days.”

In addition to the Smart Wireless solutions already installed at Ternium Siderar, Emerson offers a wide range of wireless field instrumentation and plant operations equipment, including Fisher® position monitors,  Rosemount analytical and Machinery Health™ Management devices, and native wireless interfaces to DeltaV™ digital automation systems, and SmartStart™ services.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.