Emerson to retrofit plant and turbine controls at Korea South East Power Company’s (KOSEP) Samcheonpo thermal power plant

1007-Samcheonpo

Emerson Process Management will apply its PlantWeb digital plant architecture with Ovation expert control system at units 3 and 4 of the Samcheonpo thermal power plant. The plant is owned by Korea South East Power Company (KOSEP), a major player in the Korean market.

High resolution image








MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Emerson selected for its integrated PlantWeb™ automation solution, ability to meet aggressive project schedule and prior successes in other KOSEP power plan

PITTSBURGH (July 20, 2010) — Emerson Process Management has won a contract to apply its PlantWeb digital plant architecture with Ovation expert control system at units 3 and 4 of the Samcheonpo thermal power plant, located in South Gyeongsang Province in South Korea. The six-unit, 3,240-MW plant is owned by Korea South East Power Company (KOSEP), a major player in the Korean market. The company’s power plants currently generate 7,334 MW of electricity – more than 10 percent of the country’s electric generating capacity.
 
In order to extend the service life of these units, the contract calls for replacement of outdated controls at Samcheonpo units 3 and 4 (2 X 560 MW) with Emerson’s Ovation expert control system. The Ovation system, which was designed specifically to meet the unique challenges of the power generation industry, will monitor and control each unit’s Combustion Engineering boiler, GE turbine and balance-of-plant processes. Unifying boiler and turbine operations translates into a number of significant benefits, including improved unit stability, responsiveness and thermal efficiencies; tighter overall control of plant operations; and a more concise view of key plant and turbine parameters. In all, Emerson will install 17 Ovation controllers and 52 workstations that will manage a total of approximately 21,300 I/O points. 

In addition, Emerson’s comprehensive solution for Samcheonpo units 3 and 4 includes Rosemount® instrumentation, including eight pressure transmitters and 24 differential pressure-type level transmitters, as well as vibration monitoring and protection system equipment, coal feeder controls, soot-blower optimization and a boiler tube leak detection system. Emerson will also remodel a central control room that will enable plant operators to efficiently monitor both units from one location. Equipment delivery for Unit 3 is slated for September 2010, just six months after contract award. Commercial operation for Unit 3 is expected in December 2010; Unit 4 is scheduled to return to service in March 2011.

Emerson and KOSEP have had a long, successful relationship in the power generation industry; Emerson’s technologies are already in use or being installed at numerous KOSEP plants, including Samcheonpo units 1 and 2. In fact, shortly after finalizing the contract to modernize controls at Samcheonpo units 3 and 4, the two organizations signed a Memorandum of Understanding to collaborate on the modernization of existing power plants and the construction of new plants in Korea, the Middle East, Africa, Southeast Asia and Latin America.

“Emerson offered us not only a comprehensive and integrated control solution, but also the engineering and support capabilities necessary to complete this major retrofit project on an accelerated schedule,” said Son Kwang-Sig, general manager, Power Generation Management Team, KOSEP. “The equipment and controls modernization of Samcheonpo units 3 and 4 will not only help us to greatly extend the life of these units, but also ensure that they operate at optimal efficiency and reliability.” 

“We are gratified by KOSEP’s ongoing confidence in Emerson’s people and technologies,” said Bob Yeager, president of the Power & Water Solutions division of Emerson. “We are confident that implementation of our PlantWeb technologies, along with boiler-turbine unit coordinated control, will translate into ongoing O&M savings and operational efficiencies at the Samcheonpo thermal power plant.”

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.