Emerson provides reliable and cost saving shutdown protection for underground gas storage project in China

1009-CNPC1
Emerson provides reliable and cost saving shutdown protection for underground gas storage project in China

Emerson’s Bettis PressureGuard self-contained emergency shutdown systems are protecting the Dazhangtou natural gas storage reservoir project in Tianjing, China.
High resolution image


1009-CNPC2

Emerson’s Bettis PressureGuard systems are spring based, making them ideal for remote wellhead installations where external power sources are not available.

High resolution image







MEDIA CONTACT:

Bettis™ PressureGuard™ self-contained emergency shutdown systems installed at wellhead where external power sources are not available

AUSTIN, TEXAS (September 13, 2010) -- China National Petroleum Corporation (CNPC) has selected Bettis™ PressureGuard™ self-contained hydraulic shutdown systems from Emerson Process Management for installation on the Dazhangtou natural gas storage reservoir project in Tianjing, China. Seven PressureGuard systems, which require no external power source, will protect the gas storage reservoir by closing gate valves when a high or low pressure threshold has been reached. 

The Dazhangtuo reservoir is the first gas storage facility in China. It strengthens the peak-gas adjustment capacity of the Shan-jing natural gas pipeline, which extends 585 miles from Yulin, Shanxi, to Beijing. Gas that is not needed immediately is diverted into underground storage facilities. This allows excess gas delivered during the summer to be made available to help meet the increased demand in the winter.

The Bettis PressureGuard systems are being installed in the wellhead area of the gas storage facility, where there is no electrical power. This is an ideal application for the spring-based PressureGuard shutdown systems because no plant air, fuel gas, electricity, or expensive nitrogen back-up systems are required. A self-contained oil reservoir also removes the need for any external hydraulic piping. A Pressure Pilot with Hi-Hi, Low-Low options triggers the system when a pressure threshold is reached. 

The Bettis PressureGuard system offers built-in temperature compensation and pressure relief and has proven to be highly successful in years of field service under some of the most demanding operating and environmental conditions. The actuator can be used with either rotary or linear spring-return hydraulic operators to provide a fail-safe system adaptable to ball, plug, and other quarter-turn valves as well as reverse-acting gate and other linear operated valves.             

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson Automation Solutions via
   Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.