Emerson’s Smart Wireless technology helps Atlas Pipeline - Westex improve production efficiency and save $725K on installation

Choosing wireless monitoring over a traditional wired network helped natural gas processor spend less while gaining real-time diagnostics, cutting operator rounds, and enabling affordable network expansion 


AUSTIN, Texas (October 13, 2010) — Emerson Process Management’s Smart Wireless technology saved Atlas Pipeline - Westex an estimated $725,000 in installation costs and has improved production efficiency at Atlas' Benedum natural gas processing facility near Midkiff, Texas. 

The self-organizing IEC 62591 (WirelessHART®) network connects a new plant with an older unit in the same facility.  Pulling data from the old plant into the new plant’s control room using conventional wiring was not financially feasible because of the distance and obstacles between the two plants. 

“Wireless was our only way to do this project," said Wayne Wasson of Atlas. "Without it we would have spent three times as much.” 

The wireless network includes 99 of Emerson's Rosemount® wireless temperature, pressure, level, and discrete-input transmitters that communicate with three Smart Wireless Gateways to collect real-time data from gas processing and storage tanks, cooling towers, and compressors. The majority of the wireless devices replaced local indicators in the old plant, while others measure pressure along pipes between the two plants and tank level in the new plant. 

Data from the wireless network is integrated into the plant’s DeltaV™ digital automation system, which monitors and controls critical plant processes. Atlas operators also use AMS Suite: Intelligent Device Manager predictive maintenance software to actively manage key field devices in both plants, including Fisher® valves. Predictive diagnostics provided through AMS Suite have enabled Atlas to eliminate operator rounds to the old plant, saving multiple trips per day.

“The application gave us a centralized location to view our total plant process,” said Wasson. “Our operators do not have to make rounds to learn about potential problems. They can more efficiently operate the plant by seeing changes and problems when they occur.”

The Smart Wireless network was up and running immediately after installation. It can easily be expanded with the addition of new transmitters.

 “Overall installation was easy and seamless and took about a day to have them all communicating and showing up in the DeltaV system,” Wasson said. “We’re only using one-fifth of the capacity of those gateways. It will be easy to add new points. That’s a real benefit of the self-organizing network.”​​​​​​​

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson Automation Solutions via
   Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.


Please enable JavaScript to use this website.