Emerson’s Smart Wireless network helps Northstar Bluescope Steel boost production and reduce maintenance costs

1010-Northstar1

Northstar Bluescope Steel is using Emerson’s Smart Wireless technology to monitor and control temperatures on an electric arc furnace at their facility in Delta, Ohio.
High resolution image


1010-Northstar2
Emerson’s Smart Wireless network helps Northstar Bluescope Steel boost production and reduce maintenance costs

The Smart Wireless network at Northstar Bluescope Steel includes Emerson’s Rosemount 848T high density wireless temperature transmitter.

High resolution image







MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Replacing traditional wired network with wireless solution for control and monitoring has improved operations and worker safety in harsh environment

AUSTIN, TEXAS (October 4, 2010) — Emerson Process Management’s Smart Wireless technology has helped Northstar Bluescope Steel improve furnace control at its mini-mill in Delta, Ohio.  As a result, the mill has been able to boost production by as much as one batch per day, cut maintenance costs by $200,000 annually, and improve worker safety. 

Emerson's self-organizing wireless network, based on the IEC 62591 (WirelessHART®) standard, collects data used to control the temperature of cooling panels and water-cooled burners on the mill’s electric arc furnace. This data is critical to safe furnace operation. Overheating cooling panels can lead to major furnace damage, with a blown-out panel costing as much as $20,000 to repair. Production time is also lost when the furnace must be shut down during maintenance or repairs. 

“Better temperature control through wireless has allowed us to add up to one additional batch per day,” said Rob Kearney, maintenance supervisor for Northstar Bluescope Steel. "With each batch worth as much as $200,000, that's a significant advantage."

Emerson’s wireless solution replaced a hard-wired monitoring network with hundreds of wiring junctions.  The old network suffered frequent measurement failures in the mill's harsh environment, with its high electromagnetic field, flying slag, vibration, moisture, and temperatures as high as 3,000 degrees Fahrenheit.

“Between nine and 12 measurements per week would fail due to high temperatures or physical damage to sensors, cable or conduit," said Kearney. "And when a measurement point fails, the furnace must be shut down. The new wireless solution eliminated almost 100 percent of the cable and conduit – which reduced maintenance costs by $200,000 annually.  The new wireless solution has been up and running for four months without a single failure.”

The wireless network includes 32 of Emerson's Rosemount® wireless temperature transmitters; 28 are used for control and four for monitoring. The transmitters send their data to a Smart Wireless Gateway, which interfaces with the mill’s transformer-regulation and burner-control system.

“Safety has also been improved,” Kearney said. “The furnace’s cooling panels are operating consistently at a safe temperature, and there is less maintenance required around the hot furnace shell, where ambient temperatures can be 140 degrees.”

Due to its success with Emerson's Smart Wireless, Northstar Bluescope intends to implement a similar wireless solution for a second electric arc furnace.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson Automation Solutions via
   Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.