Emerson flowmeters for marine fuel measurement help Rederi AB Transatlantic reduce costs, improve operations and increase profitability

1010-Rederi1HQ

Emerson’s Micro Motion Coriolis flowmeter, installed as part of a fuel efficiency control system, is helping Rederi AB Transatlantic maximize fuel efficiency
High resolution image


1010-Rederi2HQ

Emerson’s Micro Motion Coriolis flowmeter, installed as part of a fuel efficiency control system, is helping Rederi AB Transatlantic maximize fuel efficiency
High resolution image







MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Micro Motion® Coriolis flowmeters help Rederi AB Transatlantic maximize fuel efficiency 
and reduce fuel costs by 2 per cent per vessel, with an investment payback time of only two months

BOULDER, COLO (November 1, 2010) -- Following a joint program by Rederi AB Transatlantic, Transas AB, and Emerson Process Management to develop an onboard solution for better control of marine fuel consumption, Rederi AB Transatlantic has installed Emerson’s Micro Motion® Coriolis mass flowmeters on several ships in its fleet. The standard solution uses a compact Micro Motion F100-Series Coriolis sensor with a Model 1700 transmitter to provide highly accurate, traceable and transparent mass-based measurement of fuel oil. 

Using the MODBUS communications protocol, the mass flowmeter sends data to a fuel efficiency control system supplied by Transas AB in Sweden.  This system, also called a Conning unit, collects information from the flowmeter and other onboard systems to help the crew optimize the operation of the ship. Tighter control and management of fuel burned improves engine efficiency, delivering fuel savings and reducing emissions. 

Emerson also supplied its Mobrey MCU 901 Universal Transmitter Controllers and Indicators to show the actual flow for local reading in the engine room or control room.

According to Leif Holmberg, superintendent at Rederi AB Transatlantic, "The Coriolis mass flowmeter and Conning unit have been installed and running for over a year on the M/V Ortviken, and a slightly shorter time on the M/V Transpaper. The installations have reduced our fuel costs by approximately 2 per cent over a 12 month period for each vessel. These savings in fuel have provided a return on our total investment of just two months.” 

“Based on these successes, we will be investing in further installations onboard other ships in our fleet,” continued Holmberg. “We are also working to develop the fuel efficiency system to be even more effective in saving fuel by using additional information that other systems onboard can provide.”   

Shipping operators, including Rederi AB Transatlantic, are facing volatile fuel prices and challenging emission regulations.  These issues are compounded by the need to control costs and improve operating efficiencies. Fuel represents a major cost in the operation of a large vessel, making fuel efficiency a real focus for the shipping and marine industry. With highly accurate, continuous, and reliable measurement of fuel quality, usage costs and waste can be managed.

Micro Motion F-Series Coriolis meters are designed to provide highly accurate mass flow, volume flow, and density measurement in applications that require a compact, drainable design. Coriolis meters deliver high-accuracy direct mass, density and temperature measurement as compared with mechanical meters that measure volume flow only and have to be read manually. The Coriolis mass measurement can be directly correlated to cost and energy content of fuel, and the measurements are unaffected by changes to the flow profile and variable fuel properties such as density or viscosity. 

Micro Motion Coriolis meters are ideally suited to marine fuel measurement applications, providing extremely high accuracy and wide rangeability. They are easy to install between the Booster Module and engine, and because there are no moving parts, they also offer savings from reducing replacement or maintenance requirements when compared to volumetric flow measurement devices. 

Emerson's unique MVD Direct Connect™ architecture further simplifies installation and reduces cost and complexity through direct integration into a MODBUS host. Digital and analog communications deliver the data directly to the control room or bridge, enabling close control. This complete solution also provides access to all Micro Motion instrument variables, including embedded diagnostics and full sensor configuration.

Micro Motion devices are suitable for a range of measurement installations on cruise and ferry ships, merchant ships (including container vessels and tankers), navy ships and special purpose vessels such as ice breakers.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.