Emerson releases new railcar emergency shutoff valve

MCK 1151_N562

Fisher® Type N863 Snappy Joe Emergency Shutoff Railcar Valve provides twice the flow rate capacity of the current N562, reducing propane railcar loading/unloading time

High resolution image




Fisher® Type N863 Snappy Joe Emergency Shutoff Railcar Valve provides twice the flow rate capacity of the current N562, reducing propane railcar loading/unloading time 

McKINNEY, TEXAS (January 2, 2014) - Emerson Process Management has released the new Fisher Type N863 Snappy Joe Emergency Shutoff Railcar Valve with up to twice the flow rate of the previous N562, offering a significant reduction in propane railcar loading/unloading time.

 The Fisher railcar valve was originally developed more than 30 years ago and is the first and only Emergency Shutoff Valve (ESV) specifically designed for railcars in the propane industry. It can be used with most compressed gases such as propane, anhydrous ammonia, natural gas liquids, aerosols, etc.

The new N863 design greatly increases flow capacity, up to 413 GPM versus 200 GPM for the N562, depending on system piping and flow capabilities.  The N863 valve seals are available in Nitrile, Neoprene, Kalrez™ (FFKM), Teflon™ (PTFE), Viton™ (FKM) and EPDM to provide broad application versatility. UL Listing for the N863 is expected in 2014.

More information about the emergency shutoff valve and Fisher regulators may be found at www.fisherregulators.com or by contacting your Fisher LP-Gas Equipment Distributor.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Please enable JavaScript to use this website.