Micro Motion HFVM Viscomaster
Robust Micro Motion® viscosity meter provides reliable and repeatable measurement for demanding applications
BOULDER, COLO (March 4, 2015) -- Emerson Process Management introduces the Micro Motion Heavy Fuel Viscosity Meter (HFVM) Viscomaster, the next generation of the Micro Motion 7829 Viscomaster direct insertion viscosity and density meter. Making use of the same rugged and reliable tuning fork design as its predecessors, the HFVM incorporates a new robust low friction Diamond-like Carbon (DLC) coating that is ideal for tackling the most demanding of process applications such as marine heavy fuel oil (HFO) combustion control, marine gas oil (MGO) viscosity control and land-based fired heaters.
The head-mounted transmitter is hazardous area approved and has the flexibility to connect to control systems via a wide range of digital and analog protocols. System integration and startup commissioning costs are significantly reduced due to the support from 4-20mA, HART, Wireless HART and RS485 Modbus communications. The HFVM accepts and processes external signals from other field instrumentation such as temperature and mass/volumetric flow devices, enabling the meter to calculate and output enhanced process measurements while minimizing installation and cabling costs.
“We designed the HFVM Viscomaster to help solve problems that our customers face on a daily basis such as maximizing engine power output irrespective of fuel quality variations, optimizing HFO/MGO cut-over times and reducing fiscal exposure through improved NOx/SOx management,” said Andrew Sgro, Micro Motion density and viscosity product line manager.
The HFVM also incorporates a new diagnostic capability called Known Density Verification (KDV) that checks the meter for measurement alarm conditions, sensor integrity and the presence of coating, erosion or corrosion. This new technology expands the availability of diagnostic information in critical viscosity and density measurement applications which can result in significant maintenance costs and cycle time reductions.
Marine approvals for the meter include Lloyds, Germanischer Lloyd’s, Det Norske Veritas (DNV) and Bureau Veritas (BV).
About Emerson Process Management
Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include PlantWeb™, Syncade™, DeltaV™, Fisher®, Bettis™, Micro Motion®, Rosemount®, Daniel™, Ovation™ and AMS Suite.
About Emerson
Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2014 were $24.5 billion. For more information, visit Emerson.com.