Micro Motion F100P Coriolis flowmeter
Micro Motion® F100P and HPC010P meters allow operators to confidently measure chemical injection to ensure long term asset reliability and flow assurance
BOULDER, COLO (May 7, 2015) -- Emerson Process Management introduces the Micro Motion F100P and HPC010P Coriolis flowmeters to measure accurate flow rates for wellbore chemicals injected at high pressure conditions. Both meters are designed for demanding offshore applications that require robust performance with low maintenance needs. These meters will allow operators to confidently monitor chemical injection to ensure long term asset reliability and flow assurance.
The F100P is a 1-inch meter with a maximum pressure rating of 6250 psi (431 bar) that targets measurement for higher flow rates typical for hydrate inhibitors. The HPC010P is the first ultra-high pressure Coriolis meter developed by Emerson, and will have a maximum operating pressure of 15,000 psi (1034 bar) to address offshore chemical injection measurement for chemicals such as corrosion, scale and asphaltene inhibitors.
“These meters are breaking boundaries for Coriolis meters in high pressure applications where positive displacement meters are today’s legacy practice. Coriolis meters deliver new value to our customers through more accurate measurement and reduced maintenance over traditional PD technology,” said Michelle Marceny, specialty products business manager for Emerson’s Micro Motion business. “Coupled with Smart Meter Verification (on-line verification of meter performance), these meters provide safe, reliable and highly repeatable performance with reduced maintenance in the toughest applications.”
”The new flowmeters will help owner-operators and service companies overcome many challenges of chemical injection applications and reduce chemical costs while increasing operational efficiency and system reliability,” said Inderpreet Shoker, analyst for the ARC Advisory Group.
These flowmeters will be available starting late 2015, and are the newest addition to Emerson’s chemical injection solution capabilities which include Tescom flow control technology, Micro Motion mass flowmeters, and Rosemount® pressure and temperature transmitters.
About Emerson Process Management
Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include PlantWeb™, Syncade™, DeltaV™, Fisher®, Bettis™, Micro Motion®, Rosemount®, Daniel™, Ovation™ and AMS Suite.
About Emerson
Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2014 were $24.5 billion. For more information, visit Emerson.com.