Emerson’s Smart Wireless solutions improve wellhead and heat exchanger monitoring on StatoilHydro offshore platform

802-Statoil1

Emerson's Smart Wireless solutions have been successfully applied to the Grane platform, which is stationed in the Norwegian Sea and operated by StatoilHydro.
High Resolution Image


802-Statoil2

The Rosemount Smart Wireless pressure transmitters are used to measure pressure drop over the platform heat exchangers.
High Resolution Image


802-Statoil3

The transmitters were proven to be highly reliable in the crowded wellhead environment of the Grane platform.
Images courtesy of StatoilHydro

High Resolution Image




MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Wireless network proves highly reliable in crowded metal wellhead environment of Norwegian Sea oil platform

AUSTIN, TEXAS (February 25, 2008) –  Emerson Process Management has successfully applied its wireless self-organizing mesh field network to monitor wellhead annular pressure and heat exchanger pressures on the Grane offshore platform. The Grane platform is operated by StatoilHydro and is stationed in the Norwegian Sea off the coast of Bergen, Norway.  

Emerson's self-organizing wireless mesh technology is ideally suited to the application of wireless technology, enabling remote monitoring and control of the process in difficult to reach areas. Emerson believes that the network on the Grane platform is the first offshore wireless installation in Europe. 

"We had some concerns that this new technology would work reliably in the harsh environment of our offshore platform," said Geir Leon Vadheim, Instrument Lead, Grane Operations, StatoilHydro. "We also needed to address the issue of how we would integrate the data gathered by the wireless gateway into a third party system. As it turns out, the integration was easy and the performance of the Smart Wireless transmitters has exceeded our expectations." 

The wellhead area is crowded with metal pipe work, metal walkways above and below, together with other metal obstructions. Despite the challenging environment, as each transmitter was powered up, the devices found the gateway, and the mesh was established.  As new devices were added, they quickly and easily joined the mesh.  Signal strength and consistency during the operational period has been excellent.

The wireless network enables continuous monitoring of pressures and eliminates the need for daily visits to the wellhead to manually record gauge readings. Continuous monitoring enables unusual readings to be identified earlier and action taken to investigate and rectify faults before they develop into serious problems.

The Smart Wireless network on the platform includes 22 wireless Rosemount® pressure transmitters which replace traditional gauges.  Ten pressure transmitters are mounted on a wellhead and used to measure annular pressure. A further twelve pressure transmitters monitor inlet pressure and pressure drop over the heat exchanger. Each transmitter relays data back to the operator consoles in the control room. Installation was quick and easy with a gauge adapter fitting used to allow a direct "screw in" replacement.  A wireless gateway was mounted outside the process area on one side of the platform, at a height where it oversees the wellhead area. 

 "We are delighted with the performance of the Emerson Smart Wireless network in these challenging conditions," said Geir Leon Vadheim. "Following a short training program, our instrument engineers are very confident about adding more wireless devices to our installation as required. These typically take around two hours to install compared with up to two days for a conventional wired unit."

Following the success of this installation, StatoilHydro is planning to install Emerson Smart Wireless transmitters on other offshore platforms that it operates in the area.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson Automation Solutions via
   Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.