Emerson to Install PlantWeb® Digital Architecture with Ovation® Control System at New Illinois Power Plant

Use of digital bus-based technology expected to reduce installation and startup costs as well as long-term O&M costs at new CWLP coal-fired Dallman Power Station Unit 4


PITTSBURGH, PA (March 25, 2008) — Emerson Process Management announced today that it has been selected to install its PlantWeb® digital plant architecture with the Ovation® expert control system at Dallman Power Station Unit 4. This new 200-MW, coal-fired plant will be operated by City Water, Light and Power (CWLP), the largest municipal utility in Illinois.

The new unit, which is being built adjacent to the existing three-unit Dallman Power Station, will replace 76 MW of electricity previously generated by CWLP’s two Lakeside Station turbine generators. According to CWLP, when completed in 2010, Dallman Unit 4 will be one of the cleanest coal-fired generating units in the nation, employing low NOx burners for the boiler, a selective catalytic reduction (SCR) system for additional NOx removal, powder activated carbon injection for mercury removal, a fabric filter baghouse for fine particulate removal, a wet flue gas desulphurization (FGD) unit for SO2 removal, and a wet electrostatic precipitator to remove acid mist and ultra-fine particulate from the flue gas.

Emerson’s Ovation control system will monitor and control the new unit’s Foster Wheeler pulverized coal-fired boiler, as well as the burner management system, bottom ash handling, combustion control system, coal handling system, FGD and SCR. The Ovation system, designed to meet the specific challenges of the power generation industry, will also interface to the unit’s Toshiba turbine controls. In all, Ovation will manage 2,500 hard I/O points and 2,500 soft I/O points. The project will be engineered and installed by the Power & Water Solutions division of Emerson.

"Dallman Unit 4 is being designed and built with efficiency and environmental stewardship in mind,” said Brian Fitzgerald, CWLP’s project manager, pointing out that when completed, the new unit is expected to cost approximately 20 percent less to operate per megawatt-hour than the most efficient of the three existing Dallman units. “Emerson’s integrated digital automation system is a comprehensive solution that will not only contribute to improved operational efficiency and reduced costs, but will also support our utility-wide commitment to protecting the environment.”

Emerson’s PlantWeb digital automation solution utilizes high-speed communications networks, intelligent field devices and bus I/O technologies to help power producers reduce installation and startup costs, control critical plant processes, increase plant efficiencies and megawatt production, and realize long-term operations and maintenance savings.

Emerson will supply six redundant Ovation controllers, seven dual-monitor operator stations, one historian and AMS™ Suite: Intelligent Device Manager asset management software. For new plant construction, AMS Device Manager streamlines device configuration and commissioning for more efficient plant startup. AMS Device Manager also provides online access to instrument and valve process information, predictive diagnostic information, and automatic documentation of field device maintenance information – all contributing to ongoing efficiency of plant operations and maintenance activities.

"CWLP is among a growing number of power generators that understand the value a digital bus-based plant architecture offers – both initially through reduced startup and commissioning costs, as well as through long-term O&M savings,” said Bob Yeager, president of the Power & Water Solutions division of Emerson.

According to Yeager, since 2006 the company has been selected to install its PlantWeb® digital plant architecture with the Ovation® expert control system at 13 new coal-fired power plants in North America, all slated to go into commercial operation within the next five years. Emerson control systems are already installed in plants representing roughly 300,000 MW of generating capacity in the United States.

"In today’s marketplace, marked by evolving environmental regulations and an increased focus on the bottom line, utilities can greatly benefit from the operational results and competitive advantages that are possible with Emerson’s PlantWeb digital automation solution,” Yeager summarized. 

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.