Emerson's Smart Wireless products prevent breakdowns and lost production on rotating reactor at Coogee Chemicals in Australia

Wireless transmitters replaced wired instruments that failed frequently due to contamination entering through the connecting points for the wires.

 

AUSTIN, TEXAS (October 27, 2008) – Emerson Process Management's Smart Wireless instruments mounted on a rotating reactor at Coogee Chemical Company, Kwinana, Australia, are credited with delivering reliable pressure and temperature measurements to prevent frequent reactor breakdowns and lost production time. Control of the process and product quality are greatly improved as a result, and productivity has increased substantially since the wireless instruments were installed in late 2007, according to Noel Shrubsall, electrical project officer at the plant.

Coogee Chemicals produces a wide range of industrial, agricultural and mineral processing chemicals.  Obtaining accurate pressure and temperature data from inside the plant's rotating reactor is very important to maintaining process control, but wired instruments were not dependable in this environment, Shrubsall said. The failure of seals on the slip-rings connecting wires to the rotating equipment allowed the entry of moisture into the instruments. Unreliable temperature and pressure measurements resulted in poor control of the reactor, which had to be shut down two or three times a week.

"The Smart Wireless solution provides a means of obtaining accurate pressure and temperature measurements from the moving vessel without having to connect wires to the measurement devices," commented Shrubsall. "Wireless delivers reliability where it wasn't available before."

The installation at Coogee Chemicals consists of two wireless instruments mounted on one end of a rotating chemical reactor and transmitting pressure and temperature data continuously to a nearby Smart Wireless Gateway. The data is passed from the gateway via Modbus communications to the programmable logic controller (PLC) controlling the process. More reliable inputs enable the PLC to improve both process control and product quality.

"We are very impressed with this wireless technology, the way it communicates, and its potential for expansion," Shrubsall said.

For further information on Emerson's Smart Wireless solution, go to www.emersonprocess.com/smartwireless.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.