Emerson introduces auto-lockdown network security for the DeltaV™ digital automation system

New DeltaV smart switches provide easy to use network security

AUSTIN, TEXAS (November 18, 2008) – "Security made easy" is how Emerson Process Management refers to its newest addition to DeltaV™ security functionality.  Built into the new family of DeltaV smart switches, Emerson has added auto-lockdown security capabilities that allow a DeltaV user to automatically lock and unlock the port access of all the switches in the network.  This lockdown will disable all unused network connections (ports) on the switch.

One of the biggest security vulnerabilities in a control system is that network devices, such as Ethernet-based network switches, are located in unsecure locations out in the process – easily accessible to everyone.  Locking down switch ports will prevent accidental connection and virtually prevent the deliberate connection of an unauthorized device to the switch.

"The recommended security practice disables unused connections on network devices," says Bob Huba, product manager for DeltaV security, "This is usually done using third party IT software which creates risk of simply not doing it at all or accidentally disabling a used port. Our DeltaV one-click lockdown function makes managing network security much easier. Even a maintenance person can use the utility as part of their troubleshooting work practices."

The one-click lockdown application automatically scans the DeltaV network to find the DeltaV switches and then allows the user the choice to automatically unlock or lock the switches.  Unlocking also enables an auto-relock of the switches in 60 minutes if the user does not perform a manual relock before then.

"Our customers tell us that they do not have time to handle these security details," says Duncan Schleiss, vice president of product marketing, Emerson Process Management. "The auto-lockdown capability of the DeltaV smart switch delivers the security-out-of-the-box experience they are seeking."

These smart switches are zero configuration, plug-and-play devices in a DeltaV network. They make our system even easier to use and more reliable," continued Duncan. "We have learned from experience that people make mistakes and a mistake in a switch configuration can shut down a plant."

DeltaV switches are available in DIN rail and rack mount versions and in fixed port and modular configurations.  They provide Megabit and Gigabit speeds over wired and fiber communications.

Performing a system risk assessment and then implementing the appropriate security practices will allow the user to provide adequate and cost-effective security for the DeltaV system.  If further help is required with site-specific DeltaV security, implementation personnel in Emerson's SureService group can be contacted to provide this service.

DeltaV systems are a core component of Emerson's open standards-based PlantWeb® digital plant architecture which substantially reduces project costs, with customers typically saving over 30% on installed costs.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.



Please enable JavaScript to use this website.