Emerson's Smart Wireless network assures bitumen pipeline stays hot during ship unloading at Terminals Pty Ltd in Australia

Wireless instruments monitor heat-tracing on pipeline which must be hot to facilitate pumping.

 

AUSTIN, TEXAS (November 10, 2008) – Emerson Process Management's Smart Wireless solution was chosen by Terminals Pty Ltd to monitor temperatures in a 900-meter-long 8-inch (200mm) heat-traced pipeline used for unloading bitumen from ships at its Geelong Terminal in Australia. It is necessary to make certain the electric heaters are operating all along the pipeline to keep the bitumen hot (160°C) and fluid. If a heater fails, a cold spot could form causing the bitumen to solidify and plugging the line with expensive consequences.

"We needed to monitor the bitumen line," according to Bitumen Terminal project manager Joe Siklic, "to make the operators aware of cooling anywhere in the line from the ship to the storage facility, which could result in an emergency shutdown. Any delay in unloading could keep a ship at the pier longer than planned with demurrage costing up to $30,000 US per day."

The wireless technology was selected, Siklic said, for its lower initial cost and minimal maintenance as compared with hard wiring. Eight Rosemount® wireless temperature transmitters are evenly spaced along the pipeline, sending temperature readings on one-minute intervals to a Smart Wireless Gateway on shore that channels data to the AMS® Suite predictive maintenance software used for instrument configuration and performance monitoring. The collected data are also forwarded to a SCADA system in the terminal control center via fiber-optic cable.

Due to the self-organizing nature of this technology, each wireless device acts as a router for other nearby devices, passing the signals along until they reach their destination. If there is an obstruction, transmissions are simply re-routed along the mesh network until a clear path to the Smart Wireless Gateway is found.  All of this happens automatically, without any involvement by the user, providing redundant communication paths and better reliability than direct, line-of-sight communications between individual devices and their gateway. This self-organizing technology optimizes data reliability while minimizing power consumption.

"This is an ideal application for wireless," Siklic said. "Since numerous paths exist to carry the transmissions, the network would easily compensate for a transmitter failure, and the operators would be warned. This wireless network has proved to be reliable, compatible with existing control equipment, and cost effective. The amount of structure on the wharf is minimal, and that is another benefit."

For further information on Emerson's Smart Wireless solution, go to www.emersonprocess.com/smartwireless.

Media:
• Inquiries: AutomationSolutionsPR@Emerson.com
• Contacts: Emerson Automation Solutions Global Media Contacts

Additional resources:
• Join the Emerson Automation Solutions Community
• Connect with Emerson Automation Solutions via
   Twitter Facebook LinkedIn Google+ YouTube

About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.