Emerson's Smart Wireless network enables UK power generator to monitor treated water usage

eonkingsnorth_b-exterior_hires

E.ON Kingsnorth, a 1940MW generating facility located on the Medway Estuary in Kent, UK. 
High resolution image


eonkingsnorth_a-xmitters_hires

Emerson's Rosemount wireless transmitters provide access to flow percentage readings from nonintrusive ultrasonic flowmeters. 

High resolution image


eonkingsnorth_c-turbinehall_hires

The turbine hall houses large turbines, vast amounts of metal piping, and a number of metal walkways presenting a tough environment for wireless. 

High resolution image








MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


E.ON station pinpoints water usage using new flow data from wireless transmitters in self-organizing network

AUSTIN, TEXAS (January 21, 2009) - Emerson’s Smart Wireless technology is helping E.ON UK to accurately monitor and measure treated water usage, thus allowing trending and analysis to formulate target values at its Kingsnorth dual-fired power station. Using Emerson’s Rosemount® wireless transmitters, E.ON is now able to collect flow measurement data from new flowmeters installed throughout the turbine hall. The self-organizing wireless network delivers the data for trending in an OSIsoft PI historian which helps personnel monitor water usage within the system.

E.ON Kingsnorth, a 1940MW generating facility located on the Medway Estuary in Kent, UK, needed a solution to monitor and measure water usage within its main plant. They decided to install new non-intrusive ultrasonic flow meters to carry out this task. The high cost of wiring associated with a conventional cabled solution and a desire to embrace the very latest networking technology led E.ON to evaluate wireless technologies that could meet their needs.

“E.ON is keen to adopt the very latest technology to help improve productivity, efficiency and availability, and wireless technology provides the ideal networking solution to access the flow measurement data from the turbine building without having to install new cabling,’ said Chet Mistry, Team Leader, E.ON UK.

Having initially undertaken extensive trials of Emerson’s Smart Wireless technology, E.ON selected the Emerson solution because it offered high levels of reliability and long transmitting distance, as well as the ability to add additional devices to the network without the need for additional infrastructure.

The turbine hall at Kingsnorth is around 500m long and presents a difficult working environment for wireless as it houses large turbines, vast amounts of metal piping and a number of metal walkways that could interfere with the wireless signal. Such an environment would not be suitable for a line of sight wireless solution, but Emerson’s Smart Wireless self-organizing technology encountered no problems in terms of routing data back to the gateway or reliability of connection.

“We have great confidence in the technology. The self-organizing network provides redundant routes for the data to pass back to the gateway. The resulting wireless mesh network delivers high reliability,” said Simon Lark, C&I engineer, E.ON UK

With Emerson’s self-organizing technology, each wireless device can act as a router for other nearby devices, passing messages along until they reach their destination. If there is an obstruction, transmissions are simply re-routed along the network until a clear path to the Smart Wireless Gateway is found. As conditions change or new obstacles are encountered in a plant, such as temporary scaffolding, new equipment, or a parked construction trailer, these wireless networks simply reorganize and find a way to get their signals through.

All of this happens automatically, without any involvement by the user. This self-organizing technology optimizes data reliability while minimizing power consumption. It also reduces the effort and infrastructure necessary to set up a successful wireless network.

“We were initially a little skeptical of the claims made for wireless, especially considering the environment we would be placing it in. But installation was quick and easy and we just switched them on and they all worked,” said Simon Lark.

Fourteen Rosemount wireless transmitters have been installed to provide access to flow percentage readings from the new non-intrusive ultrasonic flow meters monitoring different sections of the turbine hall. The Rosemount wireless transmitters are transmitting flow measurement data every fifteen seconds to an Emerson Smart Wireless Gateway, situated in the main administration building on the other side of the road from the turbine hall.

“The gateway is situated in a windowless room within the main building. Despite being totally surrounded by brick walls, when switched on the wireless transmitters were all clearly visible and immediately connected to the gateway,” said Simon Lark.

Using Ethernet, the data is sent from the gateway to Emerson’s AMS® Suite predictive maintenance software, which manages the wireless transmitters and uses its OPC server to import the flow data into the PI data historian. From here operators view trends and pinpoint where any loss of flow takes place.

The fourteen transmitters took around two hours to configure and then less than six hours to fully install within the plant. In contrast, a wired solution would have taken between one and two weeks to complete.

“This initial installation of wireless is providing us with valuable experience,” said Chet Mistry. “We are now hoping to be able to use this experience to apply the technology to a range of applications including accessing valve diagnostic information.”

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson Automation Solutions via
   Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.