Emerson’s Smart Wireless network helps Bord Gáis monitor gas transmission pipeline system in Ireland

904-BordGais1

Bord Gáis’ Above Ground Installation at Middleton, near Cork, Ireland.
High Resolution Image



904-BordGais3

Rosemount wireless devices are placed in enclosures, standard practice for all instrumentation used at Bord Gáis' AGI's.
High Resolution Image






MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Wireless transmitters replace analog devices as part of the Middleton facility upgrade

AUSTIN, TEXAS (April 27, 2009) -- Emerson’s Smart Wireless technology is being used to help monitor an expansive natural gas pipeline transmission system as part of an upgrade to Bord Gáis’ Above Ground Installations in Ireland. New Rosemount® wireless devices have replaced aging hard wired devices as part of a trial to decide the future specification of such sites going forward and for other sites that are due upgrades. 

Bord Gáis is a leading Irish energy provider, wholly owned by the government of Ireland that is responsible for the supply, transmission and distribution of natural gas to over 600,000 customers. Management of the gas pipeline system is a sophisticated 24-hour operation involving constant monitoring through Supervisory Control and Data Acquisition (SCADA) systems. Gas is transmitted at high pressure, around 60 - 80 bar, from its main facilities and then at remotely located Above Ground Installations (AGIs) it is reduced appropriately to supply regional distribution points and commercial customers. Bord Gáis has in excess of 200 AGIs throughout Ireland, and at all these sites the gas lines in and out are monitored.

Existing AGI’s have between three and twelve pressure transmitters measuring both inlet and outlet pressure. The cooling effect as a result of pressure reduction is also measured using temperature transmitters. These devices are connected, by hardwiring, to an onsite Remote Terminal Unit (RTU) that transmits data back to a SCADA system Master Terminal Unit at the central monitoring station in Cork. Should thresholds be exceeded to pressure or temperature, alarms are activated. 

Bord Gáis’ Mains Renewal Programme aims to ensure that the Irish natural gas facility is one of the most modern pipeline systems in Europe. As part of the process, existing AGIs reaching the end of their lifespan are being upgraded with the latest instrumentation. One such site was at Middleton, near Cork, where a number of instruments needed to be upgraded with the latest temperature and pressure transmitters. 

When Bord Gáis looked to upgrade the facility with new instrumentation, it was decided to use a network of wireless pressure and temperature transmitters. The Middleton site is quite unusual as it is divided by a road. Although cable ducting was already in place and this could have been reused, this facility presented an excellent application to test wireless technology with a view to installing wireless at other AGI’s. 

“Having adopted GPRS (General Packet Radio Service) as a `back up’ communications technology for our RTUs, we were very comfortable with wireless,” said Frank Smiddy, communication & instrumentation engineer, Bord Gáis. “We like to think that we are very forward thinking and open to new ideas and we are always looking to improve our service using the latest technology.” 

Whenever new AGI’s are installed to support extensions to the pipeline system, or existing sites are upgraded, Bord Gáis is continually looking to minimize any installation costs. Power and data cabling are usually installed in ducting at the AGI’s. However, burying cables can prove to be costly and time consuming. For the upgrade at Middleton, wireless promised to be lower cost, offered faster installation and start up, and easy integration into the existing RTUs using Modbus serial communications.

Although there is minimal traffic on the road dividing the Middleton facility, Bord Gáis could not use a line of sight wireless solution as the signal may be interrupted by passing cars, affecting the reliability of communications. With Emerson’s self-organizing Smart Wireless technology, each measurement point has a redundant communication to the RTU via two or three routes. Wireless devices can act as a router for other nearby devices, passing messages along until they reach their destination. If there is an obstruction, transmissions are simply re-routed along the network until a clear path to the Smart Wireless Gateway is found.  As conditions change or new obstacles are encountered in a plant, such as temporary scaffolding, new equipment, or a parked construction trailer, these wireless networks simply reorganize and find a way to get their signals through.

All of this happens automatically, without any involvement by the user, providing redundant communication paths and better reliability than direct, line-of-sight communications between individual devices and a receiver. This self-organizing technology optimizes data reliability while minimizing power consumption. It also reduces the effort and infrastructure necessary to set up a successful wireless network. 

Because cabling enters into potentially explosive zones, regular checks are required of cable integrity as well as the condition of the EX barriers. This is especially important for older sites where there can be an aging cabling infrastructure. Wireless removes such concerns and reduces the number of site inspections needed. 

“Emerson’s Smart Wireless technology is ideal for site upgrades where instruments and cabling can be up to 25 years old and in need of replacing,” said Smiddy. “Installing the transmitters is very simple as the wireless devices simply replace the existing analog devices and these then connect back to a gateway that we installed within the existing instrumentation kiosk.” 

Bord Gáis was very familiar with Emerson’s Rosemount pressure transmitters and was confident that Emerson’s Smart Wireless technology would work well for this application. Having tested a number of devices on a work bench, they had no hesitation in applying the technology to the Middleton facility. 

At Middleton, Rosemount wireless transmitters include five measuring pressure, one differential pressure, and one temperature; all transmitters have been successfully installed and are sending measurements back to the control room via the RTU. The devices are placed in enclosures, standard practice for all instrumentation used at Bord Gáis AGI’s, and the Smart Wireless Gateway is positioned within the instrumentation kiosk, which is effectively a “walk in” enclosure. 

“We found that the enclosures do not interfere with the signals at all. We tested a few devices that were positioned furthest away from the gateway and these worked without any problems so we proceeded to install the rest of the transmitters,” explained Brid Sheehan, communication & instrumentation engineer, Bord Gáis. “Reliability of the wireless signal has not been an issue. We trend the wireless transmissions from the control room so we can see if there are any problems, but so far there haven’t been any.”

Emerson's Smart Wireless offering is an extension of the company’s PlantWeb® digital architecture that integrates plant and field networks of industrial Wi-Fi and WirelessHART™ components with wired devices.  End users can optimize their wireless network and train personnel using SmartStart® wireless services. AMS® Suite predictive maintenance software maximizes asset management benefits from wireless. AMS gathers diagnostics from field networks which include Rosemount and Rosemount Analytical wireless devices, wired Micro Motion® Coriolis and Daniel flowmeters, and Fisher® digital valves. Native wireless interface in the DeltaV™ or Ovation® digital automation systems bring the new process and plant information into full view for operations, maintenance, and plant management.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.