Emerson’s SmartProcess® SCR Optimization Technology helps Constellation Energy’s Brandon Shores plant save $200,000 in NOx credits

New Ovation® control strategies and SmartProcess optimization technology translate into dramatic operational, environmental and financial improvements for Brandon Shores station 

PITTSBURGH (May 19, 2009) — At Constellation Energy’s Brandon Shores station, use of Emerson’s SmartProcess® Selective Catalytic Reduction (SCR) optimization technology is translating into dramatic operational, environmental and financial improvements – including improved SCR efficiency and extended SCR regeneration cycles, a 250-ton reduction in NOx and subsequent savings of $200,000 achieved by eliminating the need to purchase additional NOx credits.

At 1,300 megawatts, Brandon Shores is the third-largest power plant in terms of owned capacity within Constellation Energy’s generation portfolio. The Brandon Shores station operates with SCR systems to reduce NOx emissions during the annual ozone season from May through September. The systems work by injecting ammonia into the flue gas to neutralize NOx. In order for the SCR to work at its target efficiency rate of 90 percent NOx reduction, the flue gas entering the SCR must be greater than 585 degrees Fahrenheit. When the flue gas falls below 585 degrees Fahrenheit, the ammonia flow rate drops, resulting in less efficient NOx reduction. If the flue gas falls below 555 degrees Fahrenheit, SCR operation stops completely. 

Flue gas temperature is greatly affected by plant load. Since Brandon Shores participates in the PJM Interconnection market for regulation and is required to closely follow fluctuating load demand, the flue gas temperature frequently dropped below 585 degrees Fahrenheit and occasionally dropped below 555 degrees Fahrenheit. The original SCR control schemes were not able to optimize the flue gas temperature and struggled to maintain the minimum SCR inlet temperature. 

Constellation needed an optimization solution that controlled the SCR inlet temperature more tightly in order to meet the SCR efficiency target of 90 percent NOx reduction. Doing so would help the plant achieve the operational flexibility required to participate in the PJM Interconnection market. 

Emerson’s solution included revising the original OEM-supplied design philosophy with advanced Ovation expert control strategies and installing SmartProcess SCR optimization technology. Ovation is used to control the plant’s boiler, burner management, data acquisition and flue gas desulphurization processes. Emerson studied the original boiler and SCR designs, as well as associated operational philosophies, and developed recommendations for improvement. Several modifications were implemented in a new Ovation strategy that provided tighter management of the economizer remix temperature throughout the entire load range by revising the control aspects of the economizer bypass and outlet dampers. This resulted in more consistent control of the SCR inlet and remix temperatures.

The SmartProcess SCR optimization technology was installed to work in conjunction with the recently modified Ovation controls to further optimize the SCR inlet temperature. SCR optimization uses fuzzy logic, advanced analytics and model predictive control to closely monitor the system and related data to predict the optimum ammonia usage and current flue gas composition, and based on this information recommend the ideal SCR performance settings. SmartProcess also automatically calculates optimal bias settings for O2, fans and dampers to provide tighter control of the inlet temperature.

Since its installation in 2006, the new Ovation advanced control strategies and SmartProcess Optimization technology have tightened control of the economizer remix and SCR inlet temperatures at higher loads and increased the SCR inlet temperature at lower loads. The improvement in SCR efficiency has resulted in a reduction in NOx generation, NOx credit purchases and ammonia usage, as well as extended SCR regeneration cycles.

Prior to implementing Emerson’s solutions, the Brandon Shores SCR that was tested operated below its targeted 90 percent NOx reduction efficiency rate for approximately 190 hours during the ozone season, emitting roughly 650 tons of NOx during that time. After installing new Ovation logic and SmartProcess technology, test results showed that the SCR operated below the 90 percent target for only 70 hours, emitting 400 tons of NOx in this timeframe. By eliminating 120 hours of operation below optimal efficiency, Constellation was able to reduce the amount of NOx generated by 250 tons. At a rate of $800 per ton, Constellation has saved $200,000 in NOx credits.

“By automatically controlling the SCR inlet temperature, the SmartProcess solution makes it possible for the plant to quickly and efficiently respond to constantly changing load demand, which is critical to our participation in the PJM Interconnection market,” explained Harry Brocato, general supervisor, engineering projects at Brandon Shores. “Emerson’s technology has enabled us to dramatically increase the amount of time we operate within the optimal parameters, which, in turn, results in a significant decrease in NOx as well as a significant cost savings.”

“Today, utilities operate in a challenging operational, environmental and financial environment,” said Bob Yeager, president of the Power & Water Solutions division of Emerson. “The key takeaway for power generators, based on Constellation’s experience at Brandon Shores, is that Emerson’s control system and optimization technology can work hand-in-hand for the benefit the environment and the bottom line.”

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.


Please enable JavaScript to use this website.