Emerson’s WirelessHART™ products monitor flow on StatoilHydro Gullfaks platforms following wireless success on company’s Grane platform

StatoilGullfaks

StatoilHydro’s Gullfaks A Platform


High resolution image



Photo © StatoilHydro








MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Production improves as Smart Wireless network automates monitoring of flow from 90 wells on 3 platforms

AUSTIN, TEXAS  (May 20, 2009) -- Using open WirelessHART™ products, Emerson Process Management’s Smart Wireless network is automating flow monitoring to increase production on the company’s Gullfaks offshore platforms in the northern part of the Norwegian North Sea. Needing a monitoring approach able to be installed without interrupting flow, operators are using wireless devices to transmit real time temperature data that indirectly monitors flow, allowing quick reaction to any loss of well pressure and maximizing throughput from the well. This installation follows the success of Smart Wireless on StatoilHydro’s Grane platform.

StatoilHydro, the leading oil and gas operator on the Norwegian continental shelf, was occasionally losing flow from the producing wells at its Gullfaks A, B and C platforms, caused by a loss of wellhead pressure. Early detection of the loss of flow is important as this enables operators to flow the well through the test separator and thus re-establish flow by reducing pressure. Bringing flow back quickly improves throughput and over time significantly increases production.

The loss of flow was very difficult to detect due to there being no existing flow-metering devices installed within the well pipes. Installing such devices for this application was not practical as this would require a complete shut down of production, which would be far too expensive in terms of lost throughput. A non-intrusive solution was required, but the introduction of new sensors brings with it the problem of connecting them back to the control room. The wellhead was already a very crowded area and for safety reasons it had to be kept as clear as possible. The introduction of additional equipment such as new cabling, cable trays and junction boxes was not possible.

In the past, StatoilHydro detected loss of flow by sending an operator to the wellhead where they placed their hand on the pipe to feel whether there was a difference between the pipe temperature and the ambient temperature. Typically well fluid is 60° C so the pipe feels warm, but should flow be interrupted it slowly drops back to the ambient temperature. Temperature readings were taken only at the start and the end of a shift, so a loss of flow could easily go undetected for long periods and production would be lost.

Needing to automate the monitoring so as to provide real-time data, while also reducing personnel presence in hazardous areas, StatoilHydro initially implemented a pilot installation on the Gullfaks A, B & C platforms. Emerson's Rosemount® 648 wireless temperature transmitters were installed to indirectly indicate flow on lines at each of forty wells. The wireless devices are used to transmit data from clamp-on temperature sensors mounted on the surface of the flow pipes.

“Installing additional wired measurement points at the wellhead would mean long cable trays and a lot of wiring,” said Anders Røyrøy, Project Manager, Research & Development Projects, StatoilHydro Norway. “Wireless offers an inherent reduction in cabling infrastructure, complexity and weight, resulting in significantly lower installation costs.”

“Because there is daily radio communication within the well area it is essential that the wireless field network can coexist without any reduction in performance,” continued Røyrøy. “We have found that Emerson’s Smart Wireless mitigates the impact of interference and the data reliability is 100%.”

In contrast with the once-a-shift manual recordings, Emerson’s wireless devices now transmit readings every 30 seconds back to the Smart Wireless Gateway. The gateway is hardwired straight into the existing control system providing operators with the real time information they need to react quickly to any change in flow.

"Emerson’s wireless transmitters have enabled the quick and reliable detection of lost flow, and the immediate action to re-establish flow has increased production significantly,” said Tormod Jenssen, Staff Engineer, Plant Integrity, Gullfaks field.

“Emerson’s wireless devices are installed very quickly,” said Røyrøy. “Typically each device takes only a matter of hours to install compared to up to two days for a conventional wired device.”

StatoilHydro has now implemented additional Smart Wireless devices on Platforms A, B and C, bringing the total to 90 wireless transmitters covering all production flow lines at Gullfaks.

“Rich process information and plant diagnostics are essential for unmanned operation and by introducing Smart Wireless transmitters to our platforms we are making broad strides towards our aims,” said Røyrøy.

Emerson's Smart Wireless offering is an extension of the company’s PlantWeb® digital architecture. End users can install either field or plant networks or both in a unified wireless approach that uses the full range consisting of unified plant and field networks.  SmartStart® wireless services are available to assist where needed. AMS® Suite predictive maintenance software maximizes diagnostics from field networks which include Rosemount® transmitters and flowmeters, and Rosemount® Analytical wireless devices, wired Micro Motion® Coriolis and Daniel® flowmeters, and Fisher® digital valves. Native wireless interface in the DeltaV™ or Ovation® digital automation systems bring the new process and plant information into full view for operations, maintenance, and plant management.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.