Emerson’s digital automation creates highly efficient new Bunge rapeseed oil processing plant in Poland

909-ZTKruszwica1

Emerson’s PlantWeb architecture has enabled ZT Kruszwica to increase production by 10%

High Resolution Image


909-ZTKruszwica2

Emerson’s DeltaV system has played a key role in helping to reduce variability within the process.
High Resolution Image


909-ZTKruszwica3

The process is fully automated using over 100 of Emerson’s Baumann and Fisher control valves and over 950 ON/OFF valves fitted with Emerson’s El-O-Matic actuators
High Resolution Image


909-ZTKruszwica4

The new ZT Kruszwica processing plant has become one of Bunge's top three most efficient vegetable oil processing sites worldwide.
High Resolution Image





MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


PlantWeb® architecture with its DeltaV™ system has increased production by 10% and reduced maintenance by 50% as compared with the old plant being replaced

AUSTIN, TEXAS (September 17, 2009) -- Emerson Process Management’s PlantWeb® digital plant architecture has enabled ZT Kruszwica, a subsidiary of Bunge - the world’s largest producer of oilseed and bottled vegetable oils - to increase production by 10%, cut maintenance costs by 50% and significantly reduce the use of utilities and raw materials at a new rapeseed oil processing plant in Kruszwica, Poland.

The new ZT Kruszwica processing plant, which has become one of Bunge's top three most efficient vegetable oil processing sites worldwide, was built to replace an outdated unit located nearby. When ZT Kruszwica was looking to fully automate the new plant, it selected an automation solution based on Emerson’s PlantWeb digital plant architecture with the DeltaV™ digital automation system and using HART® communications to network Emerson’s intelligent devices throughout the plant, including Rosemount® transmitters and Micro Motion® Coriolis flowmeters. 

“Crucial to the selection of the PlantWeb architecture was our conviction that it would deliver greater efficiency than the PLC based systems we had evaluated,” said Jacek Brauer, ZT Kruszwica, Plant Automation Specialist/Automation Project Team Leader.  When it became apparent that every single process across the plant could be controlled and configured from a single engineering station, it was an easy choice.”

Emerson’s DeltaV system has played a key role in helping to reduce variability within the process. By providing easy access to trend data, DeltaV makes it easy to spot deviations from optimum operating parameters. Using this information, ZT Kruszwica has modified and improved the algorithms run by the DeltaV system to optimize the process. As a result they have been able to run the plant closer to its maximum capacity without compromising end product quality. 

The new Kruszwica plant has seen production almost double from 700 to 1300 tons a day compared with the old plant. This has been achieved largely because of the new machinery installed, including a larger extractor. The PlantWeb architecture has also helped to increase production. With access to additional measurement data it has been possible to identify and address bottlenecks in the process, and improve output. Since its start up, production at the new plant has increased by 10% as a result of improving production processes.

AMS® Suite, a key component of Emerson’s PlantWeb digital architecture, was used prior to start up to ensure that devices were installed and configured correctly. This helped to accelerate commissioning and contributed to a highly successful start up. AMS Suite is now used to check and recalibrate level devices, identify flow meter sensor errors, and monitor the health of critical devices, especially those in hazardous areas. 

“We have installed measurement points absolutely everywhere in the process, and by using the DeltaV system we are able to quickly identify if there are any problems with individual machines such as pumps,” said Brauer.  “We do not have time to monitor all the devices individually, but we can look at measurement data trends to identify and rectify faults immediately.” 

Total maintenance costs are 50 per cent lower than for the previous plant. The new high quality measurement and control devices from Emerson have been a significant factor in this reduction as they require less servicing. The automation solution has removed the need to monitor devices manually, and new procedures have been put in place to address problems quickly and efficiently.  

 Emerson’s instrumentation and DeltaV system are helping to save energy at ZT Kruszwica. One example is the introduction of new temperature measurement points on the heat exchanger. Four Rosemount temperature transmitters are now used where previously only one was in place. The increased data made available from these additional instruments showed that the heat exchanger was only 50% efficient. Improvements were made to the program running this section of the process and efficiency was increased to 90% by using the DeltaV system.  This has seen energy reduced by 1300GJ a month which amounts to EURO 77,000 a year. 

The new plant, incorporating Emerson’s digital architecture and DeltaV, has helped save valuable resources. There has been a significant reduction in the amount of raw materials and utilities used; hexane consumption and the use of bleaching earth have been reduced by 25%. This is as a result of constantly improving the programmes run by the DeltaV system. A new closed loop system that returns water back into the process has decreased water use by 75%.

This process is fully automated by the PlantWeb architecture, using over 100 of Emerson’s Baumann™ and Fisher® control valves and over 950 ON/OFF valves fitted with Emerson’s El-O-Matic® actuators, all controlled by the DeltaV system. Utilities are measured by Rosemount Vortex and Magnetic flowmeters.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson Automation Solutions via
   Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.