Emerson’s Smart Wireless technology helps CalPortland Company comply with air quality regulations at California cement plant

910-CalPortland

Emerson's Smart Wireless technology reliably monitors the process used to reduce NOx emissions inside a rotary cement kiln at CalPortland's cement plant.
High Resolution Image








MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Self organizing wireless network reliably monitors cement kiln’s NOx emissions reduction process despite rotating equipment, harsh conditions

AUSTIN, TEXAS (October 26, 2009) – Emerson Process Management’s Smart Wireless technology has enabled CalPortland Company to comply with air quality emissions requirements at its Colton, California, cement plant, despite rotating equipment and harsh conditions.   

The CalPortland installation includes Emerson’s self-organizing wireless network of field instrumentation that reliably monitors the process used to reduce NOx emissions inside a rotating cement kiln at the facility. NOx is a byproduct of the pyro process involved in the chemical procedure of cement manufacture

The wireless network includes four of Emerson’s Rosemount® wireless temperature transmitters, one wireless DP transmitter, and a Smart Wireless Gateway. CalPortland chose wireless because it was the best solution that could meet the very challenging application. “The rotation, extreme temperature, and the location of the kiln (at 20 to 40 feet above grade), made using a wired solution impractical,” said Steve Tyrrell, CalPortland senior electrical supervisor. 

“With a rotary kiln, the continued addition of process variable instrumentation to optimize the control strategy becomes overwhelming.  The wireless option allowed for movement of the process indicators to various positions on the kiln for development of the control strategy,” continued Tyrrell. “Minimal maintenance of the wireless option also ensures reliability of the process signals for greater process control. We thought this was a perfect opportunity to apply wireless.”

The gradually-sloped 540-foot-long, 13-foot-diameter kiln rotates almost twice a minute and operates at temperatures as high as 2,800° Fahrenheit. The company uses a Selective Non-Catalytic Reduction (SNCR) process of spraying ammonia into the kiln to control NOx emissions. It needed to monitor the temperature of the ammonia, the process gases as well as the kiln’s slight vacuum. It had tried using a slip ring around the kiln to check these parameters but frictional wear ground down the ring and the growth of the kiln as it heated up broke insulators isolating the process signal.

“By installing this wireless network, we were able to monitor and treat the NOx in the kiln successfully when there was no other alternative,” Tyrrell said. “Wireless was a brilliant option for our project. This has allowed us to comply with the NOx emissions regulations and improve control over the process.”

The installation of the four devices onto the kiln was completed in one day. The DP transmitter was installed on the injection shroud to measure the extremely low vacuum inside the kiln. The temperature transmitters were installed at different locations around the kiln.

The self-organizing network transmits signals reliably to a Smart Wireless Gateway despite the fact that devices are installed at opposite sides of the kiln. The line-of-sight view is blocked at times between some devices and the gateway but no data has been lost. The gateway is integrated with the facility’s existing PLC control system.

“Our plan is to equip our second kiln at this facility with the same equipment later as market conditions dictate,” Tyrrell said.

In addition to the Smart Wireless solutions already installed at CalPortland Company, Emerson offers a wide range of wireless field instrumentation and plant operations equipment, including Fisher® position monitors,  Rosemount Analytical and Machinery Health™ Management devices, and native wireless interfaces to AMS Suite® predictive maintenance software, DeltaV™ digital automation systems, and SmartStart™ Services.  SmartWireless is an extension of Emerson’s PlantWeb® digital plant architecture.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.