Emerson’s Smart Wireless network uses new Fisher® wireless position monitors to help Harcros Chemicals monitor isolated, manual valves

910-Harcros

Emerson Process Management's network of Fisher wireless position monitors is helping Harcros Chemicals reduce inadvertent emissions and bad batches, as well as avoid the high costs of rework, clean-up, and lost materials.
High Resolution Image








MEDIA CONTACT:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com


Wireless units help Kansas facility avoid three product-release incidents and save $75,000

AUSTIN, TEXAS (October 28, 2009) - Emerson Process Management’s network of Fisher® wireless position monitors is helping Harcros Chemicals in Kansas City, Kansas monitor valves previously unconnected to the plant’s control system. The Fisher position monitors are components of Emerson’s Smart Wireless family. 

Harcros uses manual valves for sampling, directing, injection, and extraction processes at the chemical production facility. Many of the valves are in remote, hard-to-reach locations too costly to access with wires. Monitoring them was a difficult process, requiring operators to enter hazardous areas or climb ladders to check the valves’ state or position. Searching for an easier, safer way to monitor valve performance, managers at the Harcros site installed the new Fisher® 4320 wireless position monitors.

Unit manager Kevin Root said the Harcros facility has documented numerous benefits from the wireless instrument applications, and total savings were far beyond the direct cost reductions of a “no wires” installation. “This was about eliminating mistakes and increasing safety,” he said. “Wireless valve position monitoring enabled us to reduce inadvertent emissions and bad batches, as well as avoid the high costs of rework, clean-up, and lost material. Eliminating these costs, up to $25,000 per incident, not including fines, is a good thing for our plant.”

The new Fisher 4320 wireless communicating position monitor can be used to monitor the position of any valve, anywhere in the plant. The easy-to-install wireless instrument provides frequent, wireless updates about the valve’s position while reducing the time and risk associated with visual inspections. 

 At Harcros, worker safety is a primary concern, not only because of the location of the valves but because of the toxic chemicals the valves contain and control. The facility uses Propylene Oxide and Ethylene Oxide for its processing operations, and exposure to either one can irritate a person’s eyes, skin, or respiratory tract.  Leaks involving toxic chemicals can also result in expensive fines. 

Sample and drain valves, for example, are opened and purged before and after each batch. Some product may be released or leaked during this process, and a new batch begins every eight to sixteen hours. Adding twenty-two wireless position monitors to these isolated, manual valves enabled Harcros personnel to identify inadvertent emissions before they could result in costly fines or production delays. Downtime, rework, clean-up and disposal can cost the facility up to $25,000 per incident. The wireless monitor units helped Harcros avoid three “product release” incidents, saving at least $75,000, not including fines.

The Fisher wireless position monitors were easily integrated with an Emerson Smart Wireless Gateway and AMS wireless configurators to form a Smart Wireless network communicating with the sites’ existing DeltaV™ digital automation system.  The self-organizing wireless network passes signals along to the gateway, bypassing obstructions as needed. Frequent performance updates occur without any involvement by the user. With redundant communication paths, wireless networks provide better reliability than direct, line-of-sight communication between individual devices and a receiver. 

“Besides applying the Fisher wireless position monitors to more of our manual valves, we are considering Emerson Smart Wireless technology for tank level management, rail-car monitoring, and a host of temperature, pressure and flow applications at our Kansas City site,” said Lloyd Hale, director of manufacturing at Harcros Chemicals.

Fisher wireless position monitors are released and available for sale.  In addition to the Smart Wireless solutions already installed at Harcros Chemicals, Emerson offers a wide range of wireless field instrumentation and plant operations equipment, including Rosemount® wireless transmitters and analytical devices, Machinery Health™ Management devices, and wireless SmartStart™ Services.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

Please enable JavaScript to use this website.