Emerson’s Smart Wireless network boosts iron ore production by 12% at Samarco’s Germano Mine in Brazil

Reliable data fed directly into facility’s DeltaV control system protects pumps and prevents process stoppages while realizing 35% savings in installed costs compared to wired network


AUSTIN, TEXAS (November 11, 2009) – Brazilian company Samarco, one of the world’s largest exporters of iron ore pellets, has seen a 12 percent increase in production at its Germano Mine in Mariana, Brazil, with the application of Emerson’s Smart Wireless technology to improve plant availability and protect key assets. 

Emerson’s WirelessHART™ standard network uses Rosemount® wireless flow and pressure transmitters to reliably monitor the seal water injection system of a dozen centrifugal pumps that remove reject material during the iron ore refining process. Fresh water is constantly injected into the operating pumps to consolidate the pump seals and to prevent the highly abrasive reject material from coming into contact with and damaging pump axels. 

The new technology delivers accurate measurements via a Smart Wireless Gateway directly into the facility’s DeltaV™ automation system. Operators can easily review flow and pressure data through AMS™ Suite predictive maintenance software, looking for trends that indicate problems and adjusting the process or scheduling preventative maintenance before asset damage or plant stoppages occur. 

The information provided by the new technology has increased availability at the Samarco facility and given operators the ability to boost production by 12 percent. The Germano Mine produces about 20 million tons/year of iron ore pellets. 

“We can better protect our pumps from damage because we’re now able to identify potential faults in the pump seals,” said Luis Carlos, technician at the mine. “We avoid reactive maintenance and plant shutdowns. We’re also able to see how much clean water we’re using in the process.”

Prior to the installation of the Smart Wireless network, little flow or pressure data were collected from the pumps and the company experienced pump breakdowns weekly.

The self-organizing mesh network has performed reliably despite the dense concentration of pumps and pipes in the installation area and the fact that some equipment is located inside a tunnel, obstacles that would have made installing a hard-wired network difficult. Flooding, which occurs in the area during heavy rains, also would have been detrimental to a hard-wired network. 

“According to our past experience, we estimate the wireless network cost 35% less than what it would have cost us to install a hard-wired network,” Carlos said.  “Everything has been working reliably, despite the difficult environment.”

Smart Wireless is an extension of PlantWeb® digital architecture that offers solutions for field instrumentation and plant operations. In addition to the products installed at Samarco, other wireless products include Fisher® position monitors, Rosemount Analytical devices and Machinery Health™ Management transmitters, and native wireless interfaces to Ovation® digital automation systems, and SmartStart® services.

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn Google+ YouTube


About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.


Please enable JavaScript to use this website.