Sidney, Ohio, January 26, 2017 – Emerson (NYSE: EMR) announced the latest generation of its Copeland Scroll™ two-stage compressor at AHR Expo in Las Vegas. The new compressor will include an expansion in the capacity range up to 10 HP and will offer comfort and efficiency at an affordable price. The Copeland Scroll two-stage compressor has been redesigned for improved performance and reliability in residential and commercial air conditioning systems with an offering to support 1.5 to 10 ton systems.
“The Copeland Scroll two-stage compressor provides contractors with an ideal way to help homeowners get the comfort and efficiency they want at an accessible price,” said Joe Linsenmeyer, director marketing, residential air conditioning for Emerson’s Commercial and Residential Solutions platform. “And in commercial applications, this compressor will help facility managers meet the 2018 rooftop efficiency regulations at an affordable cost.”
Emerson designed the latest generation of this technology to operate at ~65% capacity, delivering efficiency gains in full-load of up to 5% and up to 5% more efficiency in part-load. These improvements are enabling affordable solutions for OEMs in 15/16 SEER applications allowing OEMs to more easily meet CEE tiers, while also providing additional comfort benefits such as better humidity and temperature control.
For more information, visit Emerson.com.
About Emerson
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.
For more information, contact:
Holly Michael
[email protected]
937-560-2855