New Emerson Corrosion Monitoring Solution Enhances Integrity Management For Remote Pipelines

The Roxar FSM Log 48 Area Corrosion Monitor

The Roxar FSM Log 48 Area Corrosion Monitor is a new pipeline integrity management system that provides permanent, continuous online corrosion and erosion monitoring, enabling operators to track localized corrosion and ensure cost-effective pipeline health. High resolution image


Roxar FSM Log 48 Area Corrosion Monitor™ detects both localized and generalized corrosion, aids in boosting pipeline availability and capacity, and delivers cost-effective monitoring 

STAVANGER, NORWAY (September 27, 2018) -
  Emerson is introducing the , a new pipeline integrity management system that provides remote, continuous online corrosion and erosion monitoring, enabling operators to track localized corrosion and ensure cost-effective pipeline health even in challenging environments. 

The Roxar FSM Log 48 - with 48 referring to the number of pins in the sensing pin matrix -  is a large-area, real-time remote pipeline monitoring solution capable of distinguishing between localized and generalized corrosion, a feature that helps reduce the need for pigging and other costlier inspection methods. The Roxar FSM Log 48 has a total cost of ownership of just one typical smart PIG run of up to 10 kilometers (although this can vary according to the PIG technology).

“Localized corrosion, when undetected, can cause pipeline failures that lead to reduced transportation availability and fines or penalties--not to mention repair costs,” said Chuck Miller, Director, Global Midstream at Emerson Automation Solutions. “The Roxar FSM Log 48 reduces these risks while delivering accurate corrosion detection in remote and hard-to-reach places, making it possible to monitor a larger area of pipeline and increasing capacity.”

The Roxar FSM Log 48 continuously monitors corrosion in remote areas using WLAN and cellular data transfer protocols and built-in solar power options that reduce maintenance and personnel requirements. Armed with comprehensive, real-time pipeline health information, operators can make better decisions about when and where to conduct pig runs, integrity digs and hydrostatic pressure tests, which helps to increase pipeline availability and transportation capacity.

The system is specifically designed to work for both uncovered and buried pipelines and is easily installed on bottom pipe sections where water collection is most likely. It can be retrofitted to existing uncovered or buried pipelines and several units can be located over a pipeline, minimizing the need for pigging to assess pipeline integrity and increasing transportation capacity.

The Roxar FSM Log 48 uses the non-intrusive field signature method, in which an electric current is fed through the monitored length of pipeline to generate an electric field. The initial measurement sequence measures the voltage drop between pairs of sensing pins installed on the external pipe wall. Later measurements are compared to the field signature, where a uniform increase in voltage drops between all pin pairs indicates generalized corrosion, and a local increase in the values indicates localized corrosion. Typical detection sensitivity for generalized corrosion is 0.1 percent of wall thickness for outer pipeline diameters between six and 48 inches.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via Twitter Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Please enable JavaScript to use this website.