Emerson adds HART® 7 to vortex flowmeters for more efficient commissioning, startup, and configuration

PROD-AS-Rosemount-VortexHART-PR

Protocol expansion for Rosemount™ 8800 Vortex flowmeters helps reduce startup costs

Protocol expansion for Rosemount™ 8800 Vortex flowmeters helps reduce startup costs

EDEN PRAIRIE, MINN  (March 1, 2016) – The ability to efficiently commission field devices reduces startup costs and schedule risk for large projects. Emerson Process Management’s line of Rosemount 8800 Vortex flowmeters now offers HART® Protocol Revision 7, which allows for easier identification in the field, commissioning, and configuration.

“Making it easier to commission and start up a facility accelerates the return on our customers’ investment,” said Mark Fleigle, vice president of technology and product development for Emerson Process Management. “The extension of HART 7 to our vortex flowmeters simultaneously adds functionality and improves usability.”

Properly identifying devices both in the field and in the control room takes the guesswork out of whether or not the correct device is being configured or commissioned. The Locate Device feature of HART 7 displays a visible code on the device’s LCD screen which allows for quick field identification.

Once connected to the device, or while viewing from the control room, Long Tag allows for a detailed device name to be viewed or loaded into the flowmeter. Long Tag support increases the character limit from the current eight character tag to 32 characters, allowing the user to create more accurate descriptions necessary to track down each unique device.

HART 7 also offers greater flexibility for device configuration. For the most up to date process information, HART 7 delivers expanded burst mode capabilities to allow the vortex meter to burst up to 8 variables and to trigger messages based on process events.

In addition to the latest HART 7 features, the 8800 Vortex flowmeter now provides Sensor Signal Strength as a display and output variable. This allows for continuous health monitoring of the flow sensor both at the device and remotely as a HART variable.

To learn more, visit EmersonProcess.com/Rosemount-8800 or review the HART revisions guide for a full overview of the latest capabilities at EmersonProcess.com/HARTrevisions.

About Emerson Process Management

Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include Bettis™, DeltaV™, Fisher™, Micro Motion™, Ovation™ and Rosemount™.

About Emerson

Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2015 were $22.3 billion. For more information, visit Emerson.com.

Habilite JavaScript para usar este sitio web.