Emerson launches new salinity system for increased flow assurance and to maximize oil & gas production

Emerson Roxar Salinity Measurement System

The Roxar Salinity Measurement System consists of a salinity sensor mounted flush with the wall of the meter. The MW resonance technology ensures an instant response to changes to conductivity of the flow stream. High Resolution Image









MEDIA CONTACTS:

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com

Through new system, operators can instantly identify changes in the flow stream, take remedial action and maximize oil & gas production

HOUSTON, TEXAS (May 2, 2017) - Emerson Automation Solutions launched the Roxar Salinity Measurement System for the sensitive, accurate and real-time measurement of saline water in gas production well streams at the Offshore Technology Conference (OTC) in Houston this week.

Through the new system, operators can instantly identify changes in the flow stream and the smallest amounts of saline water at never previously achieved levels of sensitivity. This enables the operator to take immediate remedial action to prevent threats to production, such as scaling, hydrate formation and corrosion. The onset of formation water and its salinity, if not controlled, can lead to well shutdowns and cost producers millions in unplanned shutdown time.

The system, which is a key element of the Roxar Subsea Wetgas Meter and is based on microwave (MW) resonance technology, provides quantitative and qualitative real-time salinity measurements in many types of field conditions but, particularly, in the high gas volume fraction (GVF)/wet gas flows that characterize wet gas fields.

 “With oil & gas wells being produced over a broader range of process conditions and water salinity and conductivity a key operational parameter for reservoir management and flow assurance, the timing for our new salinity system couldn’t be better,” said Patrick Babka, Vice President and General Manager Roxar at Emerson Automation Solutions. “Our new system will provide crucial decision-making information for the operator in identifying production threats; developing effective scale, corrosion and hydrate prevention strategies and improving chemical control; and maximizing oil & gas production and the field’s economics.”

The Roxar Salinity Measurement System has been designed as part of the Roxar Subsea Wetgas Meter, which provides individual flow rates of gas, condensate/oil and water. The salinity system consists of a salinity sensor mounted flush with the wall of the meter. The MW resonance technology ensures an instant response to changes to conductivity of the flow stream - in seconds not minutes - and the ability to measure water conductivity down to ± 0.1 S/m and up to 99.99% GVF and sensitivity in the range of ± 0,004 S/m. Small pockets of formation water leaking into the flow can therefore be detected instantaneously rather than in hours and days - something that no other technology has achieved to date.

Emerson conducted extensive testing of the new system internally and at the Colorado Experience Engineering Station (CEESI) in the United States based on a leading operator’s specifications. In all cases, the system was found to have the high levels of accuracy and sensitivity required.

Demonstrations of the new salinity system and the Roxar Subsea Wetgas Meter will be taking place on the Emerson Automation Solutions stand 4915 at OTC. Emerson’s Svein Eirik Monge will also be presenting a paper on the new system – ‘A New Salinity System for Formation Water Detection – Test Results & An Operator Qualification Program’ – at 11 a.m. on Thursday, May 4, 2017.

Medios de comunicación:
• Contactos: contactos de prensa para Emerson a nivel mundial

Recursos adicionales:
• Únase a la Comunidad Emerson Exchange 365
• Conéctese con la unidad de negocios de Emerson Automation Solutions por medio de X Facebook LinkedIn YouTube

Sobre Emerson 
Emerson (EMR en la bolsa de Nueva York) es una empresa global de software y tecnología que ofrece soluciones innovadoras para las industrias esenciales del mundo. A través de su cartera líder en automatización y su participación mayoritaria en AspenTech, Emerson ayuda a los fabricantes de industrias discretas, híbridas y de procesos a optimizar las operaciones, proteger al personal, reducir las emisiones y cumplir con sus objetivos de sostenibilidad. Para obtener más información, visite Emerson.com.

Habilite JavaScript para usar este sitio web.