Environmentally Friendly Emerson Industrial Refrigeration System Supports Innovation Initiatives

Dayton, Ohio, November 30, 2016 – A natural refrigerant industrial refrigeration system installed at The Helix Innovation Center is helping Emerson (NYSE: EMR) with its innovation initiatives and serving as a learning lab for the industry.

 

The Helix Innovation Center features full-scale, simulated environments, including a working commercial kitchen, a two-story residential home, a grocery store, a data center and the whole facility as a commercial building. Teams will use the facility to generate new ideas and then test them under real-world conditions.

The Helix Innovation Center’s modules, not only have multiple refrigeration and/or HVAC systems installed, they also feature condensing units located in environmental chambers to enable ambient temperature control from -30˚F to 130˚F. To cool these chambers, plus the one surrounding the 2,000 square foot home, Emerson needed 50 tons of low temp cooling capacity. Emerson created a CO2 subcritical cascade system working with an Emerson industrial HFC 134a medium temperature chiller, which resulted in a complete industrial refrigeration package. This system, which is now also the industrial refrigeration module at The Helix, allows Emerson to leverage a testing environment with real operating conditions and make final tweaks backed by proven results before going to market.

 

“Our industrial refrigeration system at The Helix is unique in that it both supports the overall innovation work of the facility and is itself a sandbox like the other modules for testing, learning and innovation,” said Rajan Rajendran, vice president, system innovation center and sustainability, Emerson’s Commercial & Residential Solutions. “Emerson is leveraging the results of testing to develop larger CO2 cascade systems to serve customers in the cold storage and food manufacturing and other industries that require low temperatures and prefer natural refrigerants for their processes.”

 

“To create the new system, the Emerson team started with its existing 400 series Vilter reciprocating compressor and updated the design to withstand the higher pressures of the CO2 system. The compressor features capacity modulation via a combination of cylinder unloading and speed ranging from 700 to 1800 RPM,” said Wayne Wehber, vice president business development, Vilter, Emerson’s Commercial & Residential Solutions. “The result is an integrated system on a common skid with a pair of two cylinder compressors working in parallel to provide 50 tons at -35°F SST +25°F SCT.”

 

The system at The Helix allowed Emerson to see the process through from design to installation, start-up and commissioning and performance testing. Developing this system first in The Helix Innovation Center posed several advantages for Emerson, including ready access to the technology for testing and on-site Emerson technicians for taking measurements.

 

Emerson plans for The Helix to be a global hub of industry education. In addition to the modules, the facility includes three learning labs and the company plans to host industry meetings and hold forums for HVACR professionals on-site.

For more information visit Emerson.com/TheHelix.

 

About Emerson 
Emerson (NYSE: EMR), headquartered in St. Louis, Missouri (USA), is a global technology and engineering company providing innovative solutions for customers in industrial, commercial, and residential markets. Our Emerson Automation Solutions business helps process, hybrid, and discrete manufacturers maximize production, protect personnel and the environment while optimizing their energy and operating costs. Our Emerson Commercial and Residential Solutions business helps ensure human comfort and health, protect food quality and safety, advance energy efficiency, and create sustainable infrastructure. For more information visit Emerson.com.

 

For more information, contact:
Holly Michael
[email protected]
937-560-2855

Habilite JavaScript para usar este sitio web.