Emerson Expands Reservoir Modeling Capabilities to Maximize Recovery

Roxar API

Roxar API enables users to tackle unique and specific challenges, immediately deploy the solutions needed and create lasting competitive advantage.
High resolution image


 

 

 

MEDIA CONTACTS:

Paul Fisher
Axiom Communications Management Ltd.
+44 (0) 1285 713 776
[email protected]

Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
[email protected]

Roxar API extensibility solution enables users to respond quickly to changing environments, customize workflows with their own IP, and analyze models in different ways

STAVANGER, NORWAY (December 19, 2016) -- Emerson Automation Solutions has launched the Roxar API (Application Programming Interface), its extensibility solution for reservoir modeling and, in particular, for its industry leading software Roxar RMS™. The Roxar API helps operators customize their workflows to achieve specific goals; improves data management capabilities with greater interoperability and flexibility; preserves vital reservoir information across multiple-stage workflows; and enables users to analyze and visualize their models in different and innovative ways for improved reservoir interpretation and increased recovery.

Using Python - a powerful but simple to use programming language - the Roxar API enables operators to integrate their own Intellectual Property into reservoir modeling workflows. In addition, applications can be written or extended to access RMS project data. This increased interoperability facilitates communication and information exchange between different software packages, ensuring maximum flexibility and expanding operators’ reservoir modeling capabilities.

“Too often in the past, reservoir modeling has been a fragmented and proprietary-dominated process with a lack of flexibility and interoperability. Vital data was often overlooked if it didn’t fit comfortably within the existing workflow,” said Kjetil Fagervik, vice president of product development and marketing of Roxar Software Solutions, Emerson Automation Solutions. 

He continues: “The Roxar API opens new possibilities for subsurface workflows, enabling users to build innovative geoscience, reservoir engineering and oilfield technology applications, adding company-specific goals to generic workflows, and unleashing new creativity in how we interpret our reservoir models.”

The Roxar API, which is complementary to RMS’s shared earth model - a single model viewed by all disciplines - can be used in an open environment to expand the capabilities of existing software or used within the RMS environment to create unique solutions. The Roxar API has been designed to be accessible to novice programmers while simultaneously offering substantial power to professional software developers. The Roxar API can be accessed from within RMS using the Python Job. This allows Python scripts to be saved with projects and used with other jobs to create repeatable RMS workflows. The scripts may be shared across multiple projects and throughout organizations as needed. 

The Roxar API can also be used to build customized, standalone programs called Roxar Apps. Roxar Apps share project data and models with RMS and give extensibility to the software. An App can be developed and customized to achieve specific goals, with the Roxar API acting as a software platform on which operators can develop proprietary, commercial, or open solutions. These solutions can then be shared within the organization or with the wider community of Roxar API application users and developers. By exploring and learning from the Python developer community, users will be able to investigate different ways of visualizing and analyzing models and data.

Emerson’s Roxar RMS reservoir characterization and modeling software includes a variety of different modules covering well correlation, mapping, structural modeling, petrophysical modeling, local model updates, facies modeling, fracture modeling, reservoir engineering and uncertainty management. The latest release, RMS 10, comes with domain improvements and enhancements to the seismic to simulation workflow; new decision-support tools for improved reservoir management; and increased user performance and productivity. Roxar seismic to simulation software solutions help operators make informed decisions across the prospect lifecycle on where to drill, what production strategies to adopt, and how to maximize oil and gas recovery from their assets. For further information on the Roxar API, visit www.Emerson.com/Roxar.

Medien:
• Kontakte: Emerson − Weltweite Medienkontakte

Zusätzliche Ressourcen:
• Werden Sie Mitglied der Emerson Exchange 365 Community
• Kontaktieren Sie Emerson über X Facebook LinkedIn YouTube

Informationen zu Emerson 
Emerson (NYSE: EMR) ist ein globales Technologie- und Softwareunternehmen, das innovative Lösungen für die essentiellsten Branchen der Welt bietet. Mit seinem führenden Portfolio im Bereich der industriellen Automatisierung und der Mehrheitsbeteiligung an AspenTech unterstützt Emerson die Hybrid-, Prozess- und Fertigungsindustrie bei der Optimierung von Betriebsabläufen, dem Schutz des Personals, der Reduzierung von Emissionen und dem Erreichen ihrer Nachhaltigkeitsziele. Weitere Informationen finden Sie auf Emerson.com.

Bitte aktivieren Sie JavaScript für diese Webseite.