Emerson Expands Reservoir Simulation Software to Help Customers Maximize Field Recovery

Tempest 8.1 provides new means of representing flow behavior in fractured wells.jpg

Tempest 8.1 provides new means of representing flow behavior in fractured wells. High resolution image







Roxar Tempest 8.1 delivers new advanced simulation techniques to accurately represent flow behavior in the vicinity of fractures along well trajectories

STAVANGER, NORWAY (October 19, 2017) -- Emerson Automation Solutions has launched the latest version of its reservoir management software suite - Roxar Tempest™ 8.1, designed to provide robust and efficient numerical solutions to support reservoir engineers in maximizing field recovery.

The release complements and enhances the advanced uncertainty analysis delivered by Ensemble Smoother Based History Matching, previously introduced in the Tempest 8.0 release, and provides new means of representing flow behavior in the vicinity of fractures. The Roxar Software Solution portfolio also now offers a complete seismic to simulation package runnable in Big Loop™ workflows for advanced decision support.

“Risk mitigation, decision support and workflow integration are at the heart of Roxar Tempest. Our latest version develops these even further,” said Kjetil Fagervik,vice president of product development of Roxar Software at Emerson Automation Solutions. “Tempest 8.1 brings reservoir engineers more tools to maximize the potential of their fields as well as enhanced field productivity thanks to greater simulation performance, improved uncertainty analysis, and a truly integrated workflow from geosciences to production. The result will be consistent reservoir understanding for a greater profitability across all field lifecycle stages.”

The new fractured well feature in the reservoir simulation module Tempest MORE within Tempest 8.1 handles the physics of the fracture-to-well connection and the multiphase flow within the fracture. The ability to do this for hundreds of wells in large full-field studies with practical run times is truly unique. Setting up fracture details is user-friendly and analyzing the results is straightforward, through both the flow rates that can be reported for individual fractures and pressures and/or flows that can be mapped over the fractures. High quality results visualization and plotting capabilities offer a quick and clear understanding of the fracturing effect.

Other simulation-related enhancements include brine tracking to follow the salinity of the water and model its effects throughout the simulation. In addition, to handle multiple independent reservoirs involving fluids displaying different thermodynamic properties within the same simulation model, multiple ‘equation of state’ regions are now supported.

Finally, Tempest 8.1 comes with advanced uncertainty analysis tools delivered through Tempest ENABLE, Emerson’s uncertainty management and history matching module. This includes new upgrades to the Roxar App Connector, such as Nexus and Petrel* components; the capacity to submit runs from a Windows workstation to a Linux cluster; and new advanced uncertainty analysis tools delivered through Tempest’s Ensemble Smoother based History Matching. Additional enhancements include user capabilities to update Roxar RMS surface files and reduce memory usage.

The Ensemble Smoother is a complementary technique to proxy-based history matching which enables conditioning on all types of data to ensure that all uncertainties are comprehensively accounted for. The result is a complete seismic to simulation package runnable in the Roxar Big LoopTM workflow, an automated workflow that tightly integrates static and dynamic domains throughout the field’s lifetime and ensures optimal consistency of the reservoir properties with the underlying geology.

Roxar Tempest, which runs on Windows and Linux and operates alongside Emerson’s reservoir characterization and modeling solution Roxar RMS, is an integrated software suite that provides a single, consistent interface and is used in hundreds of installations worldwide. All modules can be deployed as an integrated suite with a common interface, or separately within 3rd party simulation workflows. More Tempest 8.1 information here.

Medien:
• Kontakte: Emerson − Weltweite Medienkontakte

Zusätzliche Ressourcen:
• Werden Sie Mitglied der Emerson Exchange 365 Community
• Kontaktieren Sie Emerson über X Facebook LinkedIn YouTube

Informationen zu Emerson 
Emerson (NYSE: EMR) ist ein globales Technologie- und Softwareunternehmen, das innovative Lösungen für die weltweit wichtigsten Branchen bietet. Mit seinem führenden Portfolio im Bereich der industriellen Automatisierung und der Mehrheitsbeteiligung an AspenTech unterstützt Emerson die Hybrid-, Prozess- und Fertigungsindustrie bei der Optimierung von Betriebsabläufen, dem Schutz des Personals, der Reduzierung von Emissionen und dem Erreichen ihrer Nachhaltigkeitsziele. Weitere Informationen finden Sie auf Emerson.com.

Bitte aktivieren Sie JavaScript für diese Webseite.