Wintershall Deploys Emerson’s Advanced Downhole Wireless Integrity Monitoring System on Maria Field

Roxar_wipt-vertical_170920

The Roxar Downhole Sensor System. High resolution image



Latest advances of Roxar Downhole Sensor System verifies well barriers and casings without production impact for improved well integrity and offshore safety

STAVANGER, NORWAY (November 20, 2017) – Emerson’s latest Roxar Downhole Sensor System has been deployed on the Maria field offshore Norway, providing the field’s operator Wintershall with improved well integrity monitoring and offshore safety.

The latest deployment of the system - a wireless solution that delivers crucial integrity data and measures online and real-time pressure and temperature information from behind the casing in subsea production wells - follows the successful deployment of several dozen systems in other fields over the past four years, all providing crucial data to offshore operators on the status of their well barriers and casing.

The pressure and temperature monitoring system allows Wintershall to verify that the predicted pressure buildup falls within the design criteria, and an alarm trigger point is implemented in case pressures that are potentially outside the system design are reached.

The Roxar Downhole Sensor System also comes with new advances that enable operators to access online displays and trending of previously unreachable temperature and pressure subsurface data behind the well casing and achieve online integrity verification without any impact on production. The system, that has been tested at 225 degC/437 degF and can withstand pressures of up to 1 380 Bar/20 000 Psi, has already generated significant direct savings for operators, due to reduced testing requirements and more time to focus on production.

“After continued sales and further advances to the system, the Roxar Wireless Downhole Sensor Solution has reached full maturity,” said Sturle Haaland, European sales director at Emerson Automation Solutions. “The system and its track record prove yet again that Emerson has the willingness and capabilities to respond to customers’ specific demands and follow through with best-in-class technology and services to meet them. Operators will now have the information they need to make informed decisions on well integrity, adhere to regulatory requirements, ensure offshore safety, and enable their wells to produce at optimal levels.”

The added knowledge on pressure and temperature dynamics delivered by the Roxar Downhole Sensor System’s highly accurate quartz gauges in previously unreachable parts of the completion has also led to a better understanding and confidence in operators’ well integrity strategies. The system ensures that wells meet integrity monitoring standards, such as API RP90 and NORSOK D-010. The system also has a Technology Readiness Level of TRL7 as per API RP 17N “Recommended Practices for Subsea Production System Reliability, Technical Risk and Integrity Management.”

The Roxar Downhole Sensor System is powered using an inductive coupling system developed in-house with no need for batteries, making it ideal for harsh environments and the high pressure/high temperature surroundings often found offshore.

The sensor is installed externally to the steel casing and may be cemented in place in the well. Continuous power and data to and from the sensor is then transmitted wirelessly through the steel casing to ensure maximum well integrity for the life of the well and enable any anomalies to be detected early and in real-time (something that would not be the case with periodic testing). The sensor system may be placed at any depth in the well completion system and has the capability to penetrate more than one set of steel casings.

The Roxar Downhole Sensor System is an integral part of the proven Roxar Intelligent Downhole Network currently installed in thousands of wells worldwide. The addition of the system to the network requires no additional hardware to the subsea control system. For more information, visit, http://www.emerson.com/en-us/catalog/roxar-downhole-wireless.

Medien:
• Kontakte: Emerson − Weltweite Medienkontakte

Zusätzliche Ressourcen:
• Werden Sie Mitglied der Emerson Exchange 365 Community
• Kontaktieren Sie Emerson über X Facebook LinkedIn YouTube

Informationen zu Emerson 
Emerson (NYSE: EMR) ist ein globales Technologie- und Softwareunternehmen, das innovative Lösungen für die weltweit wichtigsten Branchen bietet. Mit seinem führenden Portfolio im Bereich der industriellen Automatisierung und der Mehrheitsbeteiligung an AspenTech unterstützt Emerson die Hybrid-, Prozess- und Fertigungsindustrie bei der Optimierung von Betriebsabläufen, dem Schutz des Personals, der Reduzierung von Emissionen und dem Erreichen ihrer Nachhaltigkeitsziele. Weitere Informationen finden Sie auf Emerson.com.

Bitte aktivieren Sie JavaScript für diese Webseite.