managing-manufacturing-cybersecurity-risks
Cybersecurity

Managing Cyber Risk and Threats: Returning to Foundational Principles

Fallback image
by Michael LesterDirector, Product SecurityEmerson

Every day, there is news of another cyberattack. 

Revelations of hacking from independent criminal organizations and state-sponsored groups are causing increasing levels of concern within company boards, government directorates and legislative bodies. From the SolarWinds hack that affected major companies; the Colonial Pipeline attack that disrupted oil and gas supply due to precautionary operational shutdown; and the LockBit ransomware attacks, just to name a few.

These cyberattacks are not necessarily using new attack techniques, and they are unfortunately becoming more severe and more frequent. While no manufacturing organization can guarantee it will never be affected by one, there are five foundational actions that leaders can take to reduce the risk and maintain efficient operations.

 

Engage in Business Operations Mapping

Manufacturers must map their business and manufacturing systems to each function, revenue stream or mission. This will help provide understanding and ownership of each process and achieve business continuity and resiliency objectives around cyberattacks, much like business crisis management scenarios. Typically, business operations mapping requires executive sponsorship for cross-functional stakeholders, including manufacturing operations, plant cybersecurity, IT security, manufacturing systems and enterprise systems, to participate. This can be a heavy lift, so be prepared to learn a lot and seek guidance to assist with implementing a framework approach.

 

Thoroughly Analyze Threats

Manufacturers should also perform a thorough threat analysis. It’s best practice, as part of this process, to review the  MITRE ATT&CK matrices, specifically the recently developed MITRE ICS ATT&CK Matrix, which is based on a global knowledge base of adversary tactics and techniques used in real-world attacks.

 

Assess Cybersecurity Protection

It’s important to determine and evaluate the cybersecurity controls and operations currently in place through a cybersecurity assessment or audit. This should include evaluation of three main pillars:

  1. People – focuses on upskilling for new technologies and processes
  2. Processes – the operational workflows and procedures
  3. Technology – the systems and controls in place

Technology works, but people drive success. Working with an automation technology leader like Emerson that has expertise in industrial control systems and operations will strengthen the assessment.

 

Develop A Defense Strategy

Using learnings from the threat analysis and cybersecurity assessment, companies should develop a defense-in-depth strategy to address weaknesses and mitigate risk in all operations that could be impacted by direct cyberattacks, indirect cyberattacks or loss of operational capabilities. This strategy should include a risk-based prioritization of any gaps or threats to ensure the major risks are addressed first, ensuring controls of resiliency.

Evaluating those same three pillars of people, processes and technology, we often see customers find value in seeking outside resourcing, training or upskilling their people, or changing certain processes, technological controls, systems or architectures to ensure a robust defense. The action plan should also be aligned to the organization’s business continuity and disaster recovery plans – just like an operational outage from errant systems or failed hardware, cyberattack response plans need defined, active processes with objectives focused on containment and recovery time objectives.

This defensive strategy should include planning for worst-case scenarios. For a manufacturing facility, for instance, having a clear backup plan for computer systems failing, plus hard copies of orders, labels and contacts, can be vital to keep manual operations going if computers go down. This may not be possible in every scenario, but having frequently reviewed backup and continuity plans will put companies in the right position to remain operational even in the event of a cyberattack.

 

Regularly Review and Update for Efficacy

Once the defense-in-depth strategy is in place, it should be tested and reviewed methodically, purposefully and regularly to ensure it is effective and does not jeopardize ongoing operations or introduce other risks. Roles, responsibilities, and employee training should be updated when any new practice and technology is implemented.

As the risk continues to grow, cybersecurity should be top of mind for all companies. The appropriate proactive and defensive cybersecurity operations and controls should be in place to protect important data, processes and business operations. Business leaders play a critical role in this change and by partnering with cybersecurity experts, they can take crucial steps to mitigate risk.