Emerson introduces wireless totalizing transmitter to monitor turbine meters in remote applications

705 straight
Rosemount 705 Wireless Totalizing Transmitter

Rosemount® 705 Wireless Totalizing Transmitter installs quickly to unleash average flow and volume data from any turbine meter or pulse device

SHAKOPEE, MINN (April 16, 2015) -- Emerson Process Management introduces the Rosemount 705 Wireless Totalizing Transmitter for installation on new or existing turbine meters or pulse devices to deliver average flow and totalized flow volume over time. The totalizing transmitter also delivers predictive diagnostics data to indicate instrument health and support timely maintenance to intervene on issues before they impact operations.

“Unmeasured flow and volume in turbine meter or pulse applications can impact productivity and optimization of other critical areas of production,” said Bob Karschnia, vice president of wireless at Emerson Process Management. “Locating traditional analog flow measurement has often been demanding or even impossible to implement when and where you want it. The Rosemount 705 Wireless Totalizing Transmitter answers these challenges by connecting directly to any new or existing meter or pulse device, and sending data wirelessly to eliminate cabling costs, speed installation, and enable complete process data for better decision making.”

The Rosemount 705 transmitter provides average flow rate and totalization in an operator-configurable k-factor. One second updates ensure timely information, and remote mounting of the device allows for flexible installation. The transmitter can be installed in a location convenient for the wireless signal up to 1 kilometer away.

The transmitter calculates the total from a pulse measured from 0 to 10 khz and provides an optional continuous read out display. The transmitter can be configured to reset at the unit or remotely via MODBUS, EtherNet/IP or OPC from the host system.

About Emerson Process Management

Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include PlantWeb™, Syncade™, DeltaV™, Fisher®, Bettis™, Micro Motion®, Rosemount®, Daniel™, Ovation™ and AMS Suite.

About Emerson

Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2014 were $24.5 billion. For more information, visit Emerson.com.

Voor gebruik van deze website moet JavaScript worden ingeschakeld.