Emerson introduces a new non-intrusive temperature solution that delivers accurate and repeatable process temperature measurement while simplifying design, installation and maintenance

Rosemount™ X-well™ Technology is a complete point solution for accurately measuring process temperature without the need for a thermowell or process penetration

 

AUSTIN, TEXAS (March 9, 2016) - Emerson Process Management introduces Rosemount X-well Technology, a surface sensing temperature measurement solution that eliminates the need for thermowell process penetration when measuring process temperatures in pipe applications.  This solution provides an accurate and repeatable internal process temperature measurement, while eliminating possible leak points and simplifying specification, installation and maintenance.

Rosemount X-well Technology is available in the Rosemount 648 Wireless Temperature Transmitter and Rosemount 0085 Pipe Clamp Sensor Assembly. These components work together to calculate process temperature via the transmitter’s thermal conductivity algorithm. Rosemount X‐well Technology works by measuring the pipe surface temperature and ambient temperature, and combining this information with an understanding of the thermal conductivity properties of the installation and process piping.

A major advantage of Rosemount X-well Technology is accurate process temperature measurement without requiring any intrusions or penetrations into the process, allowing for quicker and easier installation along with simplified long-term maintenance.  Users do not have to design, size or maintain thermowells.  Wake Frequency Calculations are eliminated, as well as time spent determining material compatibility, the right insertion length and the necessary profile.
With Rosemount X-well Technology, users can also add temperature measurement points without having to shut down a process.  X-well Technology can be installed with a standard pipe clamp procedure and ordinary hand tools, and does not require a skilled contractor.

“Rosemount X-well Technology is the best of both worlds as it provides an accurate process temperature similar to a thermowell while maintaining the benefits of a non-intrusive surface measurement,” said Jason Rud, senior principal design engineer at Emerson Process Management. “Current surface temperature sensing technology only provides a surface measurement that can be easily influenced by ambient temperature, while Rosemount X‐well Technology corrects for external conditions to infer the process temperature.”  

Applications that can benefit from Rosemount X-well Technology include pipelines, high velocity flows, slurries, heavy particulate fluids, wellheads, clean-in-place processes, high viscosity fluids and harsh processes in the oil & gas, chemical, refining, food and beverage, metals and mining and pulp and paper industries.

To learn more about the Rosemount X-well Technology, please visit www.EmersonProcess.com/Rosemount-Xwell

 

About Emerson Process Management

Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include Bettis™, DeltaV™, Fisher™, Micro Motion™, Ovation™ and Rosemount™.

About Emerson

Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2015 were $22.3 billion. For more information, visit Emerson.com.

Voor gebruik van deze website moet JavaScript worden ingeschakeld.