Emerson introduces wireless acoustic transmitter, helping processing plants save energy and reduce environmental impact

Rosemount708

Emerson's Rosemount 708 Wireless Acoustic Transmitter combines temperature measurement with acoustic "listening" to provide visibility into the state of steam traps and pressure relief valves.

High resolution image








MEDIA CONTACT:
Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
[email protected]

The Rosemount 708 Wireless Acoustic Transmitter provides instant and constant visibility to critical steam traps and pressure relief valves through a wireless monitoring system

NASHVILLE, TENN (October 24, 2011) - Emerson Process Management has introduced the Rosemount® 708 Wireless Acoustic Transmitter.  The new transmitter is part of Emerson’s “Smart Energy Initiative,” which combines its unmatched industrial energy expertise with advanced technologies that enable customers to lower energy costs and reduce emissions. The Rosemount 708 Wireless Acoustic Transmitter helps processing plants significantly reduce their energy expenses and environmental impact by combining temperature measurement with acoustic “listening” that provides unparalleled visibility into the state of steam traps and pressure relief valves.

Steam production is a significant operating expense for processing plants, and about 20 percent of the steam leaving a boiler is typically lost through failing steam traps. The Rosemount 708 Wireless Acoustic Transmitter provides accurate measurement and constant visibility to steam traps without the effort of a manual inspection, enabling dramatic decreases in steam trap failures and fuel cost reductions of 10-20 percent each year.

Pressure relief valves are another critical component of a plant. Manual monitoring for releases at pressure relief valves occurs periodically and does not indicate when or why a release occurred, increasing the chances of a safety, regulatory, or environmental incident. The Rosemount 708 Wireless Acoustic Transmitter provides visibility to pressure relief valves by alerting operators when a valve has opened in as little as a single second. The time-stamped alerts can be compared against process conditions or environmental reporting to help identify the root cause of a release so that preventive actions can be taken to reduce future emissions.

Backed by Emerson’s proven experience in Smart Wireless field instrumentation, the new transmitter gives operators instant visibility to all their critical steam traps and pressure relief valves through a non-intrusive,WirelessHART monitoring system. This system allows monitoring throughout the plant, even in remote and hard-to-reach locations, with greater than 99% data reliability. Real-time alerts identify which areas need attention, so operators can make informed decisions on how to act.

The Rosemount 708 Wireless Acoustic Transmitter offers a fast and easy implementation and minimal ongoing maintenance, leveraging the devices, tools, and knowledge already in the processing plant. The rugged transmitter features a 10-year battery life and engineered polymer housing that is intrinsically safe, weather proof, and chemically resistant. 

Presse :
• Contacts : Contacts presse monde pour Emerson

Ressources supplémentaires :
• Rejoignez la Communauté Emerson Exchange 365
• Suivre Emerson sur Twitter Facebook LinkedIn YouTube

À propos d’Emerson 
Située à Saint-Louis dans le Missouri (États-Unis), Emerson (NYSE : EMR) est une société internationale de technologie et de logiciels, qui propose des solutions innovantes aux industries. Grâce à son portefeuille de produits d’automatisation de pointe, dont sa participation majoritaire dans AspenTech, Emerson aide les fabricants de produits hybrides, de procédés et discrets à optimiser leurs opérations, à protéger le personnel, à réduire les émissions et à atteindre leurs objectifs de développement durable. Pour en savoir plus, rendez-vous sur Emerson.com.

Activez JavaScript pour utiliser ce site Web.