Emerson’s new butterfly valve combines cost savings with high-performance in meeting a wide variety of process application needs

Fisher8590ButterflyValve
Fisher 8590 butterfly valve

Fisher® 8590 high-performance butterfly valve features a highly optioned, single design platform that reduces engineering, installation, operational and maintenance costs

MARSHALLTOWN, IOWA (May 6, 2015) — Emerson Process Management introduces the Fisher® 8590 high-performance butterfly valve that brings a selection of disk seals, actuator designs and material combinations to meeting plant-wide throttling and on-off requirements.

Ben Fletcher, product manager at Emerson, explained the design intent behind the 8590 butterfly valve. “Our goal was to give application engineers the ability to combine a single valve platform with a selection of proven technologies to control a diverse range of CL600 process demands.”

“As an example, several dynamic disk seals are available in the 8590 design to meet temperature conditions that range from low-to-moderate up to 538°C (1000° F). Severe service and cryogenic applications can be met as well with the appropriate metal-polymeric or rugged stainless steel seal construction,” Fletcher added. “Since one valve design meets several needs, overall valve engineering, purchasing, installation, operation and maintenance costs become less. “

Utilizing a lugged body design across the CL600 size range of NPS3 – NPS24, the 8590 can incorporate a splined shaft that accepts either a spring-and-diaphragm or pneumatic piston actuator. It is also available with either a square or keyed shaft that combines with handlevers, handwheels or pneumatic piston actuators.

The pressure-assisted design of the 8590 disk seals provides tight shutoff and permits the use of smaller, less expensive actuators in meeting full ASME B16.34 shutoff capabilities.

The 8590 offers true bidirectional shutoff, which means that torque necessary to open and close the valve remains constant regardless of the differential pressure across the disk. Slam-shut conditions are not created as the disk nears its seat, which extends seal life and avoids actuator and piping damage.

Besides shutoff given by the choice of elastomer and metal disk seals, the optional ENVIRO-SEAL® packing system combines with the valve’s micro-smooth shaft surface to keep emissions below 100 parts per million (PPM). Yet another extreme 8590 capability involves sour liquids and gases, with trim and bolting materials available to comply with NACE MR0175-2002, NACE MR0175-2002-2003, MR0103, and MR0175/ISO 15156.

With a CL600 rating per ASME B16.34, the valve’s face-to-face dimensions meet EN558, API609, MSS-SP68, and ASME B16.10 standards. The valve body self-centers on the line flange bolts as a fast, accurate means of centering the valve in the pipeline.

For additional information on the Fisher 8590 high-performance butterfly valve, go to or www.Fisher.com​ contact an Emerson Process Management sales office and request product bulletin 51.6:8590.

About Emerson Process Management
Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include PlantWeb™, Syncade™, DeltaV™, Fisher®, Bettis™, Micro Motion®, Rosemount®, Daniel™, Ovation™ and AMS Suite.

About Emerson
Emerson (NYSE:EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2014 were $24.5 billion. For more information, visit www.Emerson.com.

Włącz skrypt JavaScript aby skorzystać z tej strony internetowej.