Emerson introduces new wireless transmitter that delivers two process variables in a single installation

3051S_WirelessHART_differential_L

The Rosemount® 3051S MultiVariable™ Wireless Pressure Transmitter helps users gain greater insight into their process without increasing installation costs

High resolution photo








MEDIA CONTACTS:
Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
Grace.Capwell@emerson.com

The Rosemount® 3051S MultiVariable™ Wireless Pressure Transmitter helps users gain greater insight into their process without increasing installation costs 

CHANHASSEN, MINN (April 15, 2014) – Emerson Process Management introduces the Rosemount 3051S MultiVariable Wireless Pressure Transmitter, designed to directly measure two process variables in one installation so users can gain greater insight into their process without increasing installation costs. 

The more devices there are in a facility, the greater the required cost and time investments for installation, scheduled maintenance and downtime. Now users can simplify installation and maintenance routines with the Rosemount 3051S MultiVariable Wireless Pressure Transmitter. Because the transmitter measures differential and static pressure, users can reduce pipe penetrations and impulse piping along with their associated costs. The static pressure sensor is available as either true gage or absolute which allows for reduced maintenance and calibration costs. 

Backed by Emerson’s proven experience in Smart Wireless field instrumentation, users have instant visibility to their measurements through a non-intrusive, WirelessHART® monitoring system. With Rosemount 3051S wireless transmitters, users can monitor more assets throughout their facilities with greater than 99% reliability and at 40 to 60% cost savings over wired installations. 

The Rosemount 3051S MultiVariable Wireless Pressure Transmitter delivers a decade of maintenance-free performance with a 10-year stability specification, making it the most cost effective and reliable way to monitor assets while reducing installation costs.

For more information on the Rosemount 3051S MultiVariable Wireless Pressure Transmitter, visit www.rosemount.com/3051SMVWireless

Mídia:
• Contatos: Contatos de mídia global da Emerson

Outros recursos:
• Participe da comunidade Emerson Exchange 365
• Siga a Emerson no X Facebook LinkedIn YouTube

Sobre a Emerson 
Emerson (NYSE: EMR) é uma empresa global de tecnologia e software que fornece soluções inovadoras para os clientes dos mercados industrial, comercial e de consumo. Por meio de seu portfólio de automação, que é líder de mercado, além de sua participação majoritária na AspenTech, a Emerson ajuda fabricantes híbridos, de processo e discretos na otimização de suas operações, na proteção de seus funcionários, na redução de emissões e na realização de metas de sustentabilidade. Para mais informações, acesse Emerson.com.

Ative o JavaScript para usar este site.