Emerson introduces high pressure transmitter for challenging operating environments

3051SHP
Rosemount 3051S High Static Differential Pressure Transmitter

Rosemount® 3051S High Static Differential Pressure Transmitter provides reliable flow measurement in high pressure applications

AUSTIN, TEXAS (May 11, 2015) - Emerson Process Management has introduced the Rosemount 3051S High Static Differential Pressure Transmitter, a reliable solution for critical process measurements in applications requiring high static pressure capability of up to 15,000 psi (1034 bar).

As processing applications increasingly operate in conditions with extreme pressures and temperatures, operators must vigilantly monitor equipment integrity and stability in order to prevent failures, safety hazards and decreased production. In industries such as offshore and onshore oil and gas and power generation where pressures can exceed 10,000 psi, it is critical that instrumentation be robust enough to provide accurate measurements on a consistent basis.

Emerson’s Rosemount 3051S high-pressure transmitter technology and all-welded, stainless steel design is custom-engineered to withstand extremely high static pressures. The SuperModule™ platform and coplanar design reduce potential leak points by 50 percent compared to traditional designs, ensuring the highest differential pressure measurement accuracy, field reliability and safety. Moreover the hermetically sealed SuperModule isolates the pressure sensor and electronics from harsh process and environmental conditions to optimize performance and reliability over the life of the transmitter, and is backed by a 15-year warranty.

“We developed high static pressure transmitter technology to support the higher pressure applications our customers are requesting. For example, emerging oil and gas recovery techniques used in deep-sea offshore and enhanced oil recovery operations are pushing to ever higher pressures,” said Scott Nelson, vice president and general manager of Rosemount pressure products at Emerson Process Management. “Oil and gas exploration companies working in increasingly challenging operating environments require advanced technologies that provide better process insight and help them comply with industry regulations and safety standards for high pressure applications. The durable, compact Rosemount 3051S high static pressure transmitter meets these needs.”

Traditional instrumentation used for high pressure service is large and bulky and can double or triple the footprint and weight of a typical measurement point. The Rosemount 3051S High Static Pressure Transmitter’s lightweight design and compact coplanar platform weighs 60 percent less than traditional transmitters; on a typical platform using 300-500 traditional pressure transmitters, the 3051S can help oil and gas companies reduce weight by hundreds of pounds/kilograms topside. The coplanar Rosemount 3051S High Static Pressure transmitter also integrates additional hardware such as integral manifolds into a single assembly, further reducing weight and lowering overall installation and instrumentation costs.

To learn more about the Rosemount 3051S High Static Pressure Transmitter, visit: www.EmersonProcess.com/Rosemount3051SHighPressure.

About Emerson Process Management

Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include PlantWeb™, Syncade™, DeltaV™, Fisher®, Bettis™, Micro Motion®, Rosemount®, Daniel™, Ovation™ and AMS Suite.

About Emerson

Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2014 were $24.5 billion. For more information, visit Emerson.com.

Ative o JavaScript para usar este site.