Executive Summary
As wind, solar, and battery storage grow across the UK electricity grid, maintaining frequency and voltage stability has become more challenging. The retirement of coal and nuclear generation has reduced physical inertia, while renewable variability has increased the frequency and severity of grid disturbances.
Dinorwig Power Station is one of Europe’s largest pumped storage hydro facilities and has adapted to these changes by expanding how it operates and how often it responds. Once primarily dispatched for occasional low‑frequency (LF) events, Dinorwig now supports the UK grid through a wide range of operating modes that provide inertia, fast ramping power, voltage support, and sustained frequency control.
This case study summarizes how Dinorwig’s modernized operating approach enables pumped storage hydropower to complement batteries and inverter‑based renewables; thereby, helping stabilize the grid during both routine operations and major disturbances.
Why Grid Stability Is More Challenging Today
The UK grid has undergone a fundamental transition over the past decade. As coal and nuclear power plants have been retired, the system has lost large sources of synchronous generation that once contributed rotational inertia through the “flywheel effect.”
At the same time:
- Wind and solar generation now account for a much larger share of total capacity
- Grid frequency deviations occur more often and propagate more quickly
- Operator dispatch alone is insufficient to counter rapid disturbances
Maintaining grid stability increasingly depends on resources that can respond automatically, rapidly, and repeatedly; all without relying on fuel availability, weather conditions, or slow thermal startup times.
How Dinorwig Traditionally Supported the UK Grid
For decades, Dinorwig played a critical backup role to conventional baseload generation. When frequency dropped following a disturbance, the plant’s turbine governors responded automatically, opening guide vanes according to pre‑defined droop settings and injecting power into the grid within seconds.
Typical operation included:
- Units synchronized and online in spinning reserve (“spin generate”)
- Rapid increases in output during low‑frequency events
- Relatively few frequency responses per day
This approach worked well while coal and nuclear plants supplied the majority of grid inertia.
How Dinorwig Operates on a Renewable‑Heavy Grid
As battery storage became the primary source of instantaneous frequency response, Dinorwig’s role broadened rather than diminished.
Today, Dinorwig provides:
- Physical rotational inertia by operating large synchronous machines in spin generate mode
- Fast ramping real power, transitioning from motoring or idle states to full output within seconds
- Sustained voltage and frequency support, beyond the short‑duration limits of inverter‑based resources
Unlike solar or wind generation, Dinorwig is fully dispatchable 24/7 and can rapidly transition between pumping and generating modes to either absorb excess energy or supply large blocks of power when needed.
Why Pumped Storage Complements Batteries.
Battery energy storage systems excel at providing near‑instantaneous response, but their contribution is typically limited by duration, inverter capabilities, and lifecycle constraints.
By contrast, large pumped storage hydro facilities:
- Deliver energy over much longer periods
- Provide true synchronous inertia and reactive power support
- Remain available regardless of weather or time of day
At Dinorwig, these characteristics allow pumped storage to handle sustained disturbances and large system imbalances after initial battery response has been exhausted.
What Real‑World Grid Events Reveal
As renewable penetration increased, Dinorwig’s operating profile changed dramatically. Instead of only a few low‑frequency responses per day, the plant began responding to grid events far more frequently - sometimes more than a dozen times within 24 hours.
During major UK grid disturbances:
- Multiple units were dispatched within seconds or minutes
- Units operated simultaneously in different modes to support frequency, voltage, and inertia
- All six pump‑generator units were coordinated to stabilize the system
These events demonstrated that large pumped storage plants are often the only resources capable of delivering the combination of speed, scale, and flexibility required to prevent load shedding or outages.
Why This Matters for the Future Grid
As renewable generation continues to expand and grid inertia declines, system operators need more than short‑duration response. They need dependable, dispatchable resources capable of stabilizing the grid during prolonged or cascading disturbances.
Dinorwig illustrates how pumped storage hydropower that is supported by modern control strategies can evolve from a backup asset into a cornerstone of grid stability in low‑carbon power systems.
Conclusion: Pumped Storage as a Foundation for Renewable Integration
The experience at Dinorwig Power Station shows that pumped storage hydropower remains essential in modern electricity systems. By combining large energy capacity, rapid response, and synchronous grid support, pumped storage provides services that batteries and inverter‑based renewables alone cannot sustain.
As grids transition toward higher levels of intermittent generation, pumped storage plants like Dinorwig will continue to play a central role in maintaining frequency stability, supporting voltage, and ensuring reliable power delivery.
Download the White Paper
Download the full technical white paper to explore Dinorwig’s operating modes, frequency‑response data, and real‑world grid event analysis in detail.
Learn more about pumped storage automation
For a deeper look at how modern automation solutions enable flexible, reliable pumped storage operation see Pumped Storage Hydropower Automation Solutions.