Emerson Powers Integration of a New Hyperscale Data Center

Emerson integrates an 80+ MW hyperscale data center with an existing combined‑cycle plant using advanced power and energy management for grid‑to‑chip reliability.

Executive Summary: Hyperscale Data Center Power Management Integration

Emerson is integrating a new 80+ MW hyperscale data center with an existing combined cycle power plant using the Ovation™ Automation Platform. By leveraging IEC 61850 protocols with Ovation SCADA and compact controller technology, this advanced power and energy management project will ensure seamless grid-to-chip reliability, providing a scalable foundation for mission-critical digital infrastructure without disrupting existing generation operations.

The Challenge: Bridging Industrial Power and Mission-Critical Data 

As the global digital economy accelerates, the demand for "five nines" reliability in data center power has never been higher. A leading energy provider in Asia, operating a high-efficiency 180+ MW Combined Cycle Power Plant (CCPP), faces the challenge of evolving their infrastructure to support the significant addition of an 80+ MW Hyperscale Data Center.

To facilitate this expansion, the facility requires a new substation capable of seamless communication between the existing generation assets and the data center’s critical load. The primary hurdle is integrating modern Intelligent Electronic Devices (IEDs) into a unified control architecture without disrupting existing plant operations.

The Solution: A Unified Grid-to-Data Center Architecture 

Emerson is utilizing the inherent scalability of the Ovation Automation Platform to bridge the gap between the power plant and the hyperscale facility. By treating the new substation as a logical extension of the existing plant, Emerson will ensure a "single pane of glass" view for operators.

Key technical components of the implementation will include:

  • Ovation™ SCADA server integration to help facilitate high-speed data acquisition and supervisory control for the new substation.
  • Ovation™ Compact Controller (Model OCC100) deployment for compact, powerful management of local logic and I/O.
  • IEC 61850 standardization so that the project utilizes the industry-standard protocol for substation automation to ensure seamless IED interface and interoperability, allowing for accurate data exchange.
  • Seamless plant integration of the substation directly into the existing Ovation control system architecture to eliminate data silos and reduce the complexity of the control network.

The Results: Scalable Power for a Digital Economy 

By leveraging their existing Ovation Automation Platform investment, the customer will be able to successfully transition from a traditional power provider to a critical infrastructure partner for the hyperscale market.

Mission-Critical Reliability: Enhancing grid stability ensures the 80+ MW data center maintains the constant uptime required for hyperscale operations.

  • Operational Continuity: Seamless integration will prevent any negative impacts on the existing combined cycle plant's efficiency or stability.
  • Future-Ready Scalability: The modular nature of the Ovation SCADA Server and Ovation compact controller provides a blueprint for future expansions as the data center campus grows.
  • Secure & Stable Supply: Supports and strengthens the local digital economy by providing a hardened, secure power supply to mission-critical infrastructure.

Learn More About Emerson Solutions for Data Centers

Emerson delivers a portfolio of automation technologies engineered to help data center operators strengthen reliability, streamline integration, and scale confidently as demand grows.

  • Data Center Energy Management for Microgrid & Power Islands 
    Provides intelligent orchestration across microgrids, battery energy storage systems (BESS), and other renewable or traditional assets for continuous uptime and energy optimization.
  • Microgrid Controllers 
    Delivers high‑speed local logic processing and secure I/O management, enabling precise coordination between plant assets and rapidly changing data center demand.
  • Ovation AI-Enabled Applications 
    Applies intelligent decision support to improve grid stability, forecast loading patterns, and identify anomalies for better reliability and efficiency.
  • Power and Water Cybersecurity Suite 
    Strengthens cyber resilience across OT environments with continuous monitoring, threat detection, and role‑based access controls designed to protect mission‑critical power infrastructure.

Related Data Center Case Studies

Explore other data center projects demonstrating how Emerson technologies are applied to improve energy performance and operational resilience.

Need More Information?

Learn how Emerson helps data centers meet stringent availability requirements with low-risk, unified automation technologies. Contact our data center experts to start the conversation.