Roxar™ Watercut Meter
Full‑bore meter using microwave resonance to deliver accurate water cut measurement in any flow, offering robust, drift‑free sensitivity and detecting changes as small as 50 parts per million
Key Features
- Real time, water cut measurement without the need for sampling or the separation of the oil and water
- Robust, drift free, sensitive water cut measurement utilizing microwave resonance technology
- Full bore measurement, ensuring a true representation of water cut over the full cross section of the flow
- Highly sensitive measurement, detecting and tracking water content changes as small as 50ppm
- A versatile measurement instrument, suitable for all water cut applications: upstream, midstream and downstream
- Enhanced versatility with the TopCut Feature, extending the operating range of the Roxar Watercut Meter from 0-50% water cut to an impressive 0-100% water cut, perfect for applications requiring a broader range
Frequently Asked Questions
Emerson provides continuous inline measurement of water content suitable for BS&W determination without manual sampling.
Emerson’s Roxar™ Watercut Meter delivers full-bore, real-time water cut measurement using microwave resonance technology. This technology measures the dielectric properties of the flowing oil–water mixture, allowing even very small changes in water content to be detected with high sensitivity and long-term stability. The measurement is taken across the full pipe cross-section, avoiding the uncertainty associated with localized sampling or laboratory methods. This approach is widely applied in pipelines, separator outlets, and refinery feed streams where continuous product quality monitoring is required. The measurement is suitable for fiscal-quality applications and provides drift-free performance over time.
Emerson’s Roxar™ Watercut Meter determines water cut by measuring the dielectric response of the flowing mixture using microwave resonance. The meter applies full-bore microwave resonance technology to continuously analyze oil–water mixtures inline. Water and hydrocarbons exhibit fundamentally different permittivity, so the microwave signal responds directly to changes in mixture composition, enabling accurate calculation of water fraction. The full-bore measurement ensures the result represents the entire flow, removing sensitivity to phase distribution or stratification effects. This principle is used across upstream, midstream, and downstream oil and gas processes, including separators, pipelines, and refinery systems. The technology is known for delivering stable, drift-free measurement suitable for high-value monitoring.
Slugging conditions can impact measurement stability if the flow is not sufficiently mixed, but the meter is designed to handle dynamic conditions. Emerson’s Roxar™ Watercut Meter performs high-frequency measurements, enabling it to track changes in water cut in rapidly varying flow regimes. The measurement depends on representative dielectric response, so well-mixed flow improves accuracy, while high-speed data acquisition ensures transient changes are captured rather than averaged out. This allows the meter to maintain reliable performance even during unstable flow conditions where phase distribution is changing quickly. This capability is important in upstream production systems where slugging frequently occurs. Proper installation and flow conditioning further support measurement robustness.
Condensate does not change the measurement principle, but it requires careful attention to flow conditions to ensure accuracy.
Emerson’s Roxar™ Watercut Meter measures water in condensate systems using the same microwave resonance technology as for crude oil applications. Because condensate systems tend to separate more easily, there is an increased risk of phase segregation in the pipeline, which can affect measurement representativity if the flow is not well mixed. Installing the meter in locations with good mixing, or using static mixers upstream, ensures consistent dielectric response and accurate water cut calculation. This is particularly important in gas-condensate production and transportation systems.
Proper installation design is critical to maintaining measurement quality.
Flow regime significantly impacts measurement accuracy if the flow is not well mixed before the measurement point, particularly if using a technology that only samples a small part of the flow.
Emerson’s Roxar™ Watercut Meter mitigates this through high-speed measurement and full-bore sensing. Slugging and stratified flow create uneven phase distribution across the pipe, which can bias point-based measurements, but full-bore microwave measurement reduces this effect by capturing the overall mixture. However, ensuring adequate mixing or positioning the meter appropriately is still critical to maintain representativity. This is especially relevant in upstream multiphase pipelines and unstable separator outlet conditions.
Wax and scale buildup can influence measurement accuracy but can be managed through operational and calibration strategies.
Emerson’s Roxar™ Watercut Meter uses a full-bore design that reduces sensitivity to localized buildup. Deposits can alter the effective dielectric environment seen by the sensor, introducing measurement bias, but this can be corrected using inline calibration until cleaning is performed. Preventative measures such as chemical inhibition and scheduled maintenance further reduce long-term impact. This is particularly relevant in wax-prone crude systems and scaling production environments.
If using microwave, full-bore measurement, water cut remains reliable in heavy oil systems because the measurement principle is independent of oil viscosity.
Emerson’s Roxar™ Watercut Meter uses microwave resonance to detect differences between water and hydrocarbon phases. The dielectric contrast between water and hydrocarbons persists even in heavy oil, allowing accurate measurement without requiring different calibration models for viscosity. This ensures consistent performance across a wide range of crude types. This is important in heavy oil production, thermal recovery operations, and viscous crude transportation.
Changing fluid properties can affect measurement if not compensated, but modern systems include features to manage these variations.
Emerson’s Roxar™ Watercut Meter can incorporate density input and compensation features such as AutoZero. Variations in oil density or water properties can influence dielectric behavior, but real-time adjustment of the measurement baseline maintains accuracy without requiring manual recalibration. This ensures stable performance even when fluid composition evolves over time. This is critical in well testing, blending operations, and fields with variable production conditions.
Emerson’s Roxar™ Watercut Meter is available with internationally recognized hazardous-area certifications, including ATEX, IECEx, and other country-specific approvals. These certifications confirm that the instrument meets strict safety requirements for operation in explosive atmospheres, ensuring safe integration into oil and gas facilities. The design supports installation in classified areas without compromising measurement performance or reliability. This is essential for offshore platforms, onshore production sites, and refinery environments. Compliance with ATEX and IECEx standards ensures alignment with global regulatory requirements.
The most critical installation requirement is ensuring the flow is well mixed at the measurement location.
Emerson’s Roxar™ Watercut Meter is an inline, full-bore instrument that can be installed horizontally or vertically. Accurate measurement depends on avoiding phase segregation, stagnant zones, or backflow, as these conditions can distort the dielectric response. In some cases, static mixers or proper positioning in the flowline are used to ensure homogeneous flow entering the meter. These considerations apply to oil and gas production facilities, pipelines, and refinery feed systems.
Typically, an annual service visit for troubleshooting and maintenance is recommended for Emerson’s Roxar™ Watercut Meter.
Roxar Watercut Meter is supported by a global service network, enabling regular service and technical support, to maintain optimal measurement performance over time. Routine service helps identify issues such as buildup or changing flow conditions early, while access to trained engineers ensures rapid resolution of more complex challenges. Remote support capabilities further enhance response time and reduce the need for site visits in many cases. This is especially valuable for offshore installations and remote production facilities where access may be limited. A structured service approach supports long-term reliability and operational efficiency.
Emerson's Roxar™ Watercut Meter requires minimal maintenance due to its robust design, lack of moving parts and drift-free measurement approach. The meter is designed as a low-maintenance, inline measurement solution. Its full-bore configuration reduces sensitivity to localized buildup compared to probe-based designs, while the microwave resonance principle provides inherently stable, drift-free measurement without the need for frequent recalibration. In fact, the meter does not require dynamic calibration for set-up or continued high-performance. Maintenance activities are therefore typically limited to inspection and validation. This makes it well suited to offshore and remote installations where intervention should be minimized. The design supports long-term operation with low maintenance demand.