Background
CONDITION MONITORING CASE STUDY | DISTRIBUTION & WAREHOUSE OPERATIONS

Electrical Component Manufacturer Grows its Edge Analytics Program Across Warehouse Ops with Vibration Monitoring Solution

Fallback image
PREDICTIVE PROCESS ANALYTICS AT THE INDUSTRIAL EDGE

AMS Asset Monitor cost-effectively extends online, continuous condition monitoring to an unprecedented range of assets, providing greater visibility into their health. 

EXPLORE AMS ASSET MONITOR

 

RELATED CONTENT

Top 5 U.S. Power & Utility Company Reduces Labor Costs & Improves Reliability with Wireless Vibration Monitoring & Analysis Software

Emerson’s AMS Wireless Vibration Monitors, AMS Machine Works, PeakVue Technology and more helps propel Power & Utility customer into the future. 
READ CASE STUDY

 

RELATED CONTENT

Chemical Manufacturer Avoids Dangerous Failures by Monitoring Vibration and Employing Analysis Software Tools

Emerson’s Machinery Health Software and AMS 6500 Machinery Health Monitor with embedded PeakVue Technology help refiner avoid downtime.
READ CASE STUDY

Business Results

  • Substantial reduction in production slowdowns and downtime to increase process availability
  • Issues predicted a month in advance 
  • Reduction in unplanned maintenance tasks to improve scheduling

Application

Poles are moved on rollers along rails to retrieve products from tall shelves in a warehouse. The poles move with rapid speed and acceleration. If either is reduced, production slows.

Customer

German manufacturer of industrial connectors.

Challenge

Components for manufacturing are stored in baskets held in tall bay towers that rise high above the warehouse floor. To retrieve the parts that are key to production, grabbers are raised and lowered on poles that roll on rails through the warehouse at high speeds with quick starts and stops. The rollers that hug the rails take a beating and experience wear to the plastic that touches the metal rail. Vibrations in the roller mechanics indicate that abrasion and ditches are present. 

When the wear becomes significant enough, the poles must slow or stop their retrieval duty so that the rollers can be replaced. As the team began to build a new retrieval area, they wanted to be more certain of the retrieval system. They sought a method to predict when the wear on the rollers would begin to cause the mechanisms to slow or stop the retrieval process.

Solution

After successful past experiences with this Emerson solution, the customer asked the Emerson team to implement the vibration monitoring system in a newly installed warehouse area. The goal was to be able to schedule maintenance activities by predicting roller degradation before it slowed down the part-retrieval process.

Emerson’s AMS Asset Monitor gathers data from sensors on the rollers to measure and evaluate peak-to-peak vibrations. Through the OPC/UA interface, data is sent to the area PC where data is recorded, trends are logged, and levels can be compared and alarmed as needed. 

"Vibration monitoring helps us understand the asset behavior and conditions, allowing us to schedule downtime and maintenance before an accidental event or loss of production efficiency occurs.

We also feel much better and more secure knowing the system is not running blind." - Manufacturing Manager


Emerson’s Movicon SCADA visualization software enables the team to see the data easily for planning purposes. Working together, the customer and Emerson teams created a solution that in the second test phase detected a pending roller issue one month before it would have caused failure and a process breakdown. Bolstered by this success, the maintenance team now plans repairs rather than being surprised and having to interrupt production. 

Another savings came when, equipped with data, the customer team could prove a roller quality issue to the bay system manufacturer. The manufacturer of the bay system then replaced the rollers at their cost.

 

"It helped us a lot in quality issue discussions to have recorded data showing the behavior related to rising vibration levels. The data helped us understand the machine behavior and the roller conditions, and it made the manufacturer of the highbay racking system replace the rollers at their cost." - Maintenance Manager

 

The customer has seen and documented the successes and has plans to apply the Emerson solution to other retrieval areas in the warehouse as well as in other production warehouse facilities globally.

Get Started

Request a consultation to discover how Emerson's team of condition monitoring experts can help you initiate, expand, or improve your current program or projects.

Featured Products