Background
Chemical

Gas Supplier Improves Billing Accuracy with Rosemount™ MultiVariable™ Technology

Results

  • Improved billing accuracy
  • Improved reliability, safety & uptime
  • Simplified installation and reduced cost
Fallback image
Highly Reliable

Rosemount 3051S MultiVariable Transmitter provides real time, fully compensated mass flow measurement, reducing sources of traditional DP flow​ uncertainty.

Fallback image
Accurate Billing For Customers

The gas supplier was pleased with the results of improved accuracy of billing and increased reliability.

Customer

A major supplier of gases and gas handling equipment to Taiwan’s chemical industry​

Application

Gas flow metering

Challenge

Taiwan's extensive industrial base requires gases to be supplied from bulk stations or from gas processing equipment on site. Such gases are critical to the operation of the gas supplier’s customers and many need accurate flow meters to control the process and to meter the amount of gas they use.

In this industry, the predominant concern is accuracy of billing. Other concerns include reliability, safety and uptime. The gas supplier had used many different flow metering technologies in the past without complete satisfaction, including but not limited to thermal mass flow meters, turbine meters and rotameters. Gas flow metering is difficult due to small line size applications, which are prone to flow errors caused by pipe internal diameter (ID) uncertainty and orifice plate misalignment. Also, varying pressures and temperatures coupled with low flowrates provide an added challenge. The pressure and temperature variations affect all of the flow equation parameters: discharge coefficient, velocity of approach factor, gas expansion factor, bore diameter, differential pressure and density.

 

 

Solution

Emerson engineers provided the gas supplier with a highly reliable solution involving orifice plates with the Rosemount™ 3051S MultiVariable Flow Meter. The flow meter solution combines the Rosemount 1195 Integral Orifice Primary Element with the Rosemount MultiVariable Transmitter, providing a completely assembled, ready-to-install flow meter, reducing cost and simplifying installation.

Orifice technology is proven with well established standards that both suppliers and customers can agree upon. This technology is reliable, increasing uptime and safety. Due to the low flow rates and small line sizes, the Rosemount 1195 Integral Orifice Primary Element was provided. The honed body of the integral orifice reduces ID uncertainty. Also, the self-centering design eliminates plate misalignment.

The MultiVariable transmitter measures process pressure, temperature and differential pressure simultaneously and dynamically calculates 'real time', fully-compensated mass flow. Fully compensated mass flow reduces sources of traditional DP flow uncertainty caused by pressure and temperature variation.

The MultiVariable flow meter delivers unprecedented mass flow accuracy of ±0.9% over 14:1 flow turn-down. For the gas supplier, this performance means reduced variability and improved reliability and safety.

The gas supplier’s staff used the PC-based Engineering Assistant software package and handheld HART® Communicator to configure the MultiVariable transmitter . The configuration software package contains a built-in physical property database so configuration was quick and easy.

Engineers at the gas supplier were impressed with the results of improved accuracy of billing and increased reliability, safety, and uptime. Along with the ease of installation, the Rosemount MultiVariable Transmitter ensured accurate billing for their customers.