Emerson’s New Temperature Transmitter Delivers Superior Accuracy, Stability, Diagnostic Coverage and Usability

Fallback image

The Rosemount™ 3144S Temperature Transmitter improves ease of use with plug-and-play configuration, a large backlit display, and Bluetooth® wireless connectivity. High resolution image

Rosemount 3144S Temperature Transmitter offers 0.05-degrees Celsius accuracy, 20-year stability, advanced diagnostics and enhanced ease-of-use with new ReadyConnect Technology for efficient and safe operations

SHAKOPEE, Minn. (Aug. 19, 2025) – Today Emerson announced the release of the Rosemount™ 3144S Temperature Transmitter, a new industrial measurement solution with the flexibility to meet the most demanding temperature measurement challenges, allowing for increased efficiency, safety and profitability.

Today’s technicians and managers expect temperature measurement technology to be highly accurate and reliable. Instances of a measurement point performing erratically or failing can have a major impact on productivity. Greater ease-of-use is also critical as the process industry workforce transitions to more recent hires, with fewer employees overall.

The Rosemount 3144S Temperature Transmitter addresses these issues with 0.05 degrees Celsius (0.09 Fahrenheit) of accuracy needed for processes that require the highest measurement performance. It is available with an optional 20-year stability specification and a 20-year limited warranty, assuring that it is one of the most reliable solutions on the market.

Emerson’s new ReadyConnect™ Technology allows ease-of-use by enabling plug-and-play sensor configuration with a push of a button, eliminating the need to manually input sensor information and Callendar-Van Dusen coefficients, saving configuration and commissioning time.

“The Rosemount 3144S Temperature Transmitter fits well in a wide variety of applications across a broad range of industries, making it a versatile choice for many different types of temperature measurement needs,” said Ryan Leino, senior product manager with Emerson’s measurement solutions business.

An operator interface with a simplified, task-based menu and common navigation structure across host and configuration tools also allows further ease-of-use. To further increase productivity, Quick Service Buttons provide local access to basic commissioning and maintenance tasks, such as viewing the current configuration, performing a loop test and rotating the display. Bluetooth® wireless technology provides remote access to the device at distances up to 50 feet for increased productivity, reliability and safety.

To address thermowell challenges, the Rosemount 3144S Temperature Transmitter greatly expands the application coverage of Rosemount X-well™ Technology, Emerson’s non-intrusive measurement solution, which can now measure up to 650 degrees C (1,202 degrees F).

With the Loop Integrity diagnostic and RTD Measurement Protection, the transmitter provides full diagnostic coverage from the temperature sensor to the control room, including sensor health diagnostics, dual input capabilities, and continuous electrical loop monitoring, enabling real-time insight into each measurement point.

Loop Integrity performs continuous monitoring of the entire electrical loop to detect potential failures before they occur, while RTD Measurement Protection will seamlessly switch from a 4-wire to a 3-wire RTD sensor input configuration if one of the four sensor wires becomes broken, corroded, or loose anywhere from the sensor element to the transmitter terminal connections.

Learn more at www.Emerson.com/Rosemount3144S.

The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc.

Media:

Additional resources:


About Emerson
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.