Emerson’s New Data Acquisition Solutions Streamline Testing for Entry-Level Ethernet Systems

Fallback image

Emerson's NI™ Ethernet cDAQ chassis deliver high-performance, TSN-enabled synchronization in a modular, scalable platform—providing engineers with a cost-effective solution for distributed data acquisition. High resolution image

Latest addition to NI CompactDAQ lineup delivers powerful Ethernet tools and FlexLogger enhancements, providing cost-effective option for high-performance testing

AUSTIN, Texas (Feb. 18, 2025) – Emerson today unveiled the latest additions to its data acquisition (DAQ) lineup, introducing the NI™ cDAQ-9187 and cDAQ-9183 Ethernet chassis and NI 9204 input module. Along with a GitHub repository for NI FlexLogger™ DAQ software plug-ins, these new solutions provide cost-effective options for deploying high-performance test and measurement systems over Ethernet.

The cDAQ-9187 and cDAQ-9813 chassis are the first entry-level Ethernet solutions in Emerson's NI CompactDAQ family of hardware. These budget-friendly chassis are specifically designed for electrical and sensor measurements over Ethernet-supported distances. Both models feature a single Ethernet port and omit external trigger lines, reducing cost without sacrificing performance, and include QR codes for quick access to “getting started” videos and relevant documentation to help streamline the setup process.

The accompanying NI-9204 ±10-volt input module offers a lower channel count and a more affordable alternative to one of Emerson’s most popular DAQ modules. It supports both differential and single-ended channel configurations, includes multiple gain settings, and features a 16-bit analog-to-digital converter to deliver precise, reliable measurements. Engineers can build higher channel systems with Emerson’s advanced NI synchronization technology and IEEE 802.11AS-compatible switches, or by connecting the new entry-level solutions at the end of a daisy-chain of chassis.

“Our NI hardware and software advancements provide engineers with tools that enable better research, improved product quality and greater innovation,” said Jesse Lyles, vice president of semiconductor validation and electronics for Emerson’s test and measurement portfolio business. “From optimizing for cost-effective sensor measurements to enhancing workflows through customizable software, Emerson is focused on meeting the evolving needs of engineers in the test and measurement space.”

To further enhance its software portfolio, Emerson has also introduced a plug-in repository for its NI FlexLogger data acquisition software on GitHub. This open-source platform allows test engineers to download, upload and share custom plug-ins, extending the functionality of NI FlexLogger for diverse application needs. The repository includes templates and contributions from Emerson engineers and the broader user community, enabling faster development and improved test processes, enhanced functionality, and easier integration into existing NI FlexLogger setups.

To improve the availability of its test and measurement offerings, Emerson supports perpetual licensing for NI FlexLogger software. Customers now have the flexibility to choose between subscription and perpetual purchase options, allowing them to select the model that best aligns with their business needs.

*Git™ is a trademark of Software Freedom Conservancy, Inc., corporate home of the Git Project, in the United States and other countries. GitHub is a registered trademark of GitHub, Inc.

Additional resources:


About Emerson
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.