Emerson Advances Software-Defined Automation with Latest Control System Release
DeltaV™ version 16.LTS delivers software-defined capabilities to reduce automation costs, enhance operational intelligence, improve data visibility across the enterprise and strengthen cybersecurity. High resolution image
DeltaV version 16.LTS accelerates the path to an OT-ready enterprise operations platform to seamlessly integrate and optimize industrial operations
AUSTIN, Texas (Jan. 20, 2026) – Emerson, a global automation leader, has enhanced its DeltaV™ Automation Platform through the release of version 16 of its Distributed Control System (DCS) and integrated Safety Instrumented System. DeltaV version 16.LTS delivers software-defined capabilities that reduce automation costs, enhance operational intelligence, improve data visibility across the enterprise and strengthen cybersecurity. This long-term support (LTS) release consolidates new field-proven capabilities in a single release.
“The speed of technological innovation and rise of industrial AI coupled with growing compute demands at the control layer have created an inflection point requiring a new way for companies to unify operational data and scale automation across the enterprise,” said Nathan Pettus, president of Emerson’s process systems and solutions business. “DeltaV version 16.LTS is the next step in delivering the software-defined enterprise operations platform that will meet those needs, unlocking unlimited flexibility and future proofing technology choices for years to come.”
With enhanced modularity and flexibility, DeltaV version 16.LTS enables efficient deployment and expansion of automation systems. This includes access to the DeltaV IQ Controller, a fault-tolerant, modular, software-defined controller deployed in a server-based environment and able to handle the most demanding process control applications. In addition, Emerson’s flexible subscription model, DeltaV Flex System, provides companies with full DeltaV DCS capability that allows companies to pay for utilization over time and scale up or down quickly as market factors dictate.
DeltaV version 16.LTS also integrates intelligence via more seamless data and I/O connectivity enabled by next-generation field networks, providing increased intelligence to optimize and maintain assets and processes. Native support for PROFINET over Ethernet-APL on the DeltaV PK Controller enables high-speed connectivity to field devices in demanding environments across process and hybrid manufacturing operations.
DeltaV Continuous Historian Elite software builds on the power of Emerson’s AspenTech product portfolio to deliver an enhanced data foundation for enterprise-wide optimization. Creating seamless connectivity between the DCS and enterprise data management solutions, Continuous Historian Elite allows contextualized data to flow freely across the enterprise to power analytics and AI.
Enhancements to DeltaV Live continue to provide an expanded, cohesive view of operations by streaming data through the DeltaV Edge Environment to support enterprise-level decision-making and situational awareness. The new DeltaV Live Enterprise View allows secure, read-only access to displays outside of the control room, making it possible to serve control room data to enterprise-level consumers for trending and continuous improvement of operations. Enhancements also include web application integration that empowers users to bring third-party software applications—such as optimization tools—natively into the DeltaV control interface.
DeltaV version 16.LTS will also maintain its International Society of Automation (ISA) System Security Assurance (SSA) Level 1 (L1) certification. ISA SSA L1 certification provides third-party assurance of secure-by-design practices that meet ISA/IEC-62443-3-3 and 4-1 requirements.
Media:
- Contacts: Emerson Global Media Contacts
Additional resources:
- Join the Emerson Exchange 365 Community
- Visit Emerson’s Industrial Software Page on LinkedIn
- Visit Emerson’s DeltaV Automation Platform Page on LinkedIn
- Connect with Emerson via X Facebook LinkedIn YouTube
About Emerson
Emerson (NYSE: EMR) is a global automation leader delivering solutions for the most demanding technology challenges. Headquartered in St. Louis, Missouri, Emerson is engineering the autonomous future, enabling customers to optimize operations and accelerate innovation. For more information, visit Emerson.com.