CPS Energy Modernizes SCAADA to Transform Gas Distribution
Alex Solis of CPS Energy discussed how the nation’s largest municipal utility boosted the performance and reliability of its gas distribution system. A lapse in operations can mean no power or gas for residents around the region, and in South Texas, no one wants to endure the heat without power. So, when it came time to modernize its 10-year-old SCADA system, the company had a lot of considerations to address. These days, CPS Energy is well equipped to handle any situation that may occur in its gas distribution system, and residents of the region can count on their utilities being available.