7 Risk-Based Cybersecurity Best Practices for Power and Water Suppliers
Cybersecurity

7 Risk-Based Cybersecurity Best Practices for Power and Water Suppliers

Fallback image
by Bob YeagerPresident, Power and Water Solutions Emerson

Digital transformation offers significant benefits for the power and water industries. 

Advanced technologies – including the convergence of information technology (IT) and operational technology (OT), enhanced connectivity, and expanded data access – have revolutionized how utilities and municipalities automate and optimize operations, safely manage distributed energy resources, and maintain reliable, low-cost power generation and clean water production. 

However, this transformation also creates new vulnerabilities. As power and water suppliers digitize, they face escalating cybersecurity risks – especially without the right security approach and trusted partner support. 

Today, cybersecurity attacks against critical infrastructure are growing. The U.S. Environmental Protection Agency released a memorandum stressing the need to audit security practices of local water systems and Dragos – a leader in industrial cybersecurity – reported a continued increase in instances across the energy sector. 

And as attacks grow, so do costs. In fact, global annual cybersecurity attacks and threats are estimated to have cost the world $10.5 trillion annually through 2025, up from $3 trillion in 2015. 

With more distributed energy resources (DERs) like wind farms, solar facilities and microgrids supplying renewable power to the grid, which powers critical infrastructure, there is an even greater potential for hackers to remotely disrupt the flow of electricity. According to research from the U.S. Department of Energy's Argonne National Laboratory, distributed energy resources pose unique cybersecurity challenges due to their high penetration, multiple administrative domains, and increased attack surface through interconnected networks – requiring security to be designed as a core component of DER integration. 

Why It Matters: Cybersecurity threats to critical infrastructure are escalating and power and water utilities need for a structured, risk-based approach to protect operations, minimize downtime and maintain customer trust. 

  1. Cybersecurity is a moving target: Attacks evolve faster and more frequently than defenses. A static approach won't work.
  2. Risk-based strategy beats comprehensive coverage: Focus investments on the vulnerabilities most likely to harm your business – not every possible threat.
  3. Automation and control system excellence are your edge: Purpose-built solutions like Emerson's Ovation™ Automation Platform (DHS-certified) seamlessly integrate OT security into operations without sacrificing uptime or agility. 

So, as hackers today become smarter, use more sophisticated techniques, and – in many cases – evolve and innovate faster than the companies they target, the question becomes: What can companies do to fend them off? 

 

A Risk-Based Approach to Cybersecurity

Regardless of industry, adopting a risk-based approach can help you identify potential vulnerabilities and protect your company from them now and in the future. A risk-based approach is not to protect against all threats but to identify potential vulnerabilities and make strategic decisions based on the likelihood and impact of each vulnerability. 

As you bolster your cybersecurity efforts, consider these practices to ensure your approach is holistic and constantly evolving: 

Best Practice #1: Assess risk

Risk assessments equip your company with critical insights that help mitigate risks upfront. By conducting an assessment, you determine the readiness of key cybersecurity elements – including network security, data management, perimeter protection and more – and establish a better understanding of your system’s overall security posture. 

Best Practice #2: Tighten system access

Security measures can be cumbersome and may make limited security tempting, but attackers are counting on it. Keep system access tight by ensuring employees are conscientious of security policies, constantly evaluating risks and helping to build the right culture of security internally. 

Best Practice #3: Establish strong policies

Even the most sophisticated, secure measures can be rendered useless due to human error. That’s why it’s critical to educate and empower employees with strong administrative policies that reduce risks from social engineering, phishing and related attacks. 

Best Practices #4: Upgrade your control system

Downtime is costly and should be avoided as much as possible. By applying timely patches and system upgrades, you can minimize downtime while eliminating the risk of having unprotected servers and workstations.  

Best Practices #5: Go beyond perimeter protection

Attackers will often assume perimeter protection is in place and therefore use common protocols and known service ports to compromise control system components. To tackle targeted attacks, control the system perimeter and protect potential entry points by deploying customizable, adaptable firewalls and continually scanning for security gaps. 

Best Practice #6: Keep remote access in the right hands

Almost all control systems are deployed with some type of remote connectivity – but just because remote access is the norm, doesn’t make it a safe practice. On systems where remote access is a must, make sure it’s monitored and implemented securely. You may even consider multiple layers of authentication for added security. 

Best Practice #7: Know your control system

After you’ve developed and deployed your risk-based approach to cybersecurity, ensure you’re constantly monitoring risks along the way and identifying potential attacks and threats as soon as possible. The right approach to cybersecurity is one that constantly evolves and adapts. 

 

For power companies or municipal utilities looking to innovate and keep pace with competitors today, digital transformation is no longer a “nice to have” – it’s nonnegotiable. And while there can be risks, they shouldn’t stop companies from reaping rewards like enhanced collaboration and innovation among their workforce, breakthrough operational improvements and more. 

Plus, in the ever-evolving landscape of cybersecurity, the above practices are just a starting point. To truly optimize their operations and risk-based approach to protecting them, power and water companies today are automating and seamlessly integrating industry-leading cybersecurity solutions – like Emerson’s Ovation™ Automation Platform that is both Designated and Certified as Qualified Anti-Terrorism Technology by the U.S. Department of Homeland Security – into their businesses. 

Regardless of where a company is in its cybersecurity journey, there are always opportunities to improve, evolve and strengthen defenses. Emerson's risk-based approach – combined with industry-leading automation and control system solutions – helps power and water suppliers detect vulnerabilities, minimize downtime and operate with confidence. detect vulnerabilities, minimize downtime and operate with confidence.

Ready to assess your cybersecurity posture? Explore Emerson's Ovation™ control system and OT security resources to get started.