USA, Oregon, Portland
Industrial Automation & AI

How AI-Powered Automation Unlocks LNG's Clean Energy Potential

Liquefied natural gas (LNG) is a highly efficient, reliable, clean energy alternative with plentiful reserves worldwide. It's also significantly less costly to produce than most other fossil fuels.

But realizing LNG's full potential requires overcoming critical operational and infrastructure challenges.

 

The LNG Challenge

Extreme conditions and remote locations create operational complexity. Natural gas must be cooled to a consistent -260° F for liquid transport, and many reserves are located in areas where super-freezing isn't easy or convenient to maintain. As global demand for LNG rises annually, so does complexity and risk.

At Emerson, we see these issues as inspiration for innovation. We’re helping the LNG industry overcome them, applying our automation technologies, services and expertise so we all can take better advantage of this clean, cost-effective fuel source. Our experts and solutions are mitigating project risks and reducing complexity, while optimizing operations worldwide.

Energy is a complex industry that requires innovative thinking and creative solutions. When it comes to the temperature and pressures of LNG, that complexity comes into sharper focus. 

 

The Solution

Emerson technologies and experts work with companies every day to implement and monitor solutions that make it possible to safely process and transport LNG from remote, hard-to-reach locations to centralized production hubs to where it is needed most helping meet demand for clean, reliable energy.

The reliability of these gathering systems and the efficiency of experts managing the process are critical to safely optimize production. Emerson sensors and remote monitoring capabilities give experts real-time, 24/7 access to diagnostics that help keep assets running smoothly. These leading technology applications make it possible for the right experts to securely access this vital data from 300 miles offshore or anywhere else in the world.

 

Supporting Complex LNG Operations 

Emerson’s LNG technologies are providing never-been-done-before solutions to some of the top energy companies. For example, when an international energy giant looked to tap into one of the world’s major offshore natural gas reserves located offshore from Western Australia in a remote region, they set out to build a new and modern floating production facility, rivaling the size of six aircraft carriers combined. 

And when they needed industry-leading automation solutions for this ambitious project, they turned to Emerson, which served as main automation contractor on the project, responsible for process control and monitoring technologies to help the facility operate safely and reliably.

This LNG project and countless others are empowering Emerson to help companies leverage capabilities and realize new opportunities to make the most of our resources. We see opportunities to make this cleaner fuel source more widely available to meet our world’s energy needs.

Learn more about how we’re helping companies implement this energy source.