Emerson’s New Pressure Transmitter Delivers Increased Performance, Flexibility and Operational Insights
The Rosemount™ 4051S Pressure Transmitter provides 20-year warranty and stability, comprehensive diagnostics and enhanced ease-of-use. High resolution image
Emerson's Rosemount™ 4051S Pressure Transmitter provides real-time control in some applications, eliminating the need for a separate device, such as a programmable logic controller. High resolution image

Rosemount 4051S Pressure Transmitter Overview | Emerson
The Rosemount™ 4051S Pressure Transmitter is engineered to give customers more insights, more performance and more flexibility. Video Link
Rosemount 4051S provides 20-year warranty and stability, comprehensive diagnostics, and enhanced ease-of-use
SHAKOPEE, Minn. (Oct. 23, 2025) – Today Emerson announced the release of the Rosemount™ 4051S Pressure Transmitter, a new industrial measurement solution with the flexibility to meet the most demanding pressure measurement challenges by increasing performance and operational insights.
This innovative pressure transmitter can provide local real-time control, eliminating the need for a separate device, such as a programmable logic controller. This functionality is provided by two relay switches, each of which can be configured to provide on/off control of pumps, motors, and other equipment. These switches can also provide alerts based on pressure, flow, totalized flow, level, volume, or module temperature.
“The Rosemount 4051S Pressure Transmitter is designed to provide exceptional versatility and performance, helping customers improve operations and expand their pressure measurement capabilities across a broad range of industrial applications,” said Nathan Stokes, vice president pressure products with Emerson’s measurement instrumentation business.
Engineered to withstand the toughest processes and the harshest environments, with a 20-year warranty and 20-year stability specification, both unique to the pressure transmitter market. Fast response time of 40 milliseconds allows the 4051S to be used in the most demanding applications. A best-in-class 800:1 turndown ratio reduces the number of unique models needed to be kept in stock, streamlining inventory.
Advanced diagnostics provide more insights, with loop integrity continuously monitoring the health of the entire electrical loop to detect potential failures. Plugged impulse line detection alerts plant personnel so they can take action, and the transmitter can also diagnose other abnormal conditions, such as cavitation, using its built-in process intelligence. Built-in calibration and diagnostic logs provide the information needed to optimize maintenance and perform root cause analysis.
The graphical, backlit display is larger than previous models, making it easier to read and allowing inclusion of more descriptive warning messages, an always-on process variable value, and a customizable secondary area. The display can be configured in seven languages, and the intuitive user interface speeds and simplifies operator interactions, while reducing the risk of errors.
Bluetooth® connectivity from up to 50 feet (15 meters) away improves safety by allowing plant personnel to access the transmitter so they can avoid entering hazardous areas. This fast and easy connectivity increases productivity, reliability, and safety by simplifying operator rounds. Configuration and troubleshooting are improved because operators are informed as to which devices need attention, and the AMS Device Configurator mobile app provides a seamless experience across all devices.
Guided proof testing and logging simplifies these tasks with a step-by-step process. Built-in proof testing provides reliable verification of instrument functionality to improve operational efficiency and safety, and the transmitter is certified to Safety Integrity Level 2/3 and IEC (International Electrotechnical Commission) 61508. Partial proof testing includes in-situ capability allowing you to extend proof test intervals without applying an external pressure source.
Learn more at www.emerson.com/Rosemount4051S
The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc.
Media:
- Contacts: Emerson Global Media Contacts
Additional resources:
- Join the Emerson Exchange 365 Community
- Connect with Emerson via X Facebook LinkedIn YouTube
About Emerson
Emerson (NYSE: EMR) is a global automation leader delivering solutions for the most demanding technology challenges. Headquartered in St. Louis, Missouri, Emerson is engineering the autonomous future, enabling customers to optimize operations and accelerate innovation. For more information, visit Emerson.com.